Op de Next-Gen Life Science Automation onderzoekt Festo nieuwe oplossingen voor medische technologie en laboratoriumautomatisering. Op de Hannover Messe 2026 demonstreren Festo en Fraunhofer IPA de constructie van een cassette voor de processtap van het modificeren van cellen in CAR-T celtherapie. Automatisering vermindert de productietijden en -kosten aanzienlijk, waardoor op maat gemaakte kankertherapieën sneller, goedkoper en voor meer patiënten beschikbaar worden. Persbericht lezen Afbeelding Festo SE & Co. KG 2026/04/15 | Wereldwijd Celtherapieën op maat voor de behandeling van ... Op de Next-Gen Life Science Automation onderzoekt Festo nieuwe oplossingen voor medische technologie ... Persbericht lezen
Compact, customised manifold plates for precise fluid control: Diffusion Bonded Manifolds enable individualised, contamination-free fluidic solutions using an adhesive-free joining process. The technology complements existing standard components and is aimed in particular at applications in medical technology, diagnostics, laboratory automation and food analysis. Persbericht lezen Afbeelding Festo SE & Co. KG 2026/02/24 | Wereldwijd Diffusion Bonded Manifolds: Precise fluidic ... Compact, customised manifold plates for precise fluid control: Diffusion Bonded Manifolds enable ... Persbericht lezen
Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to be able to offer manufacturers of medical and laboratory equipment solutions from a single source. To this end, Festo is taking over the production systems and processes for manufacturing these complex plastic manifolds from Carville, a leading company in this field. Persbericht lezen Afbeelding Festo SE & Co. KG 2024/06/06 | Wereldwijd Festo Expands its Portfolio with Multilayer ... Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) ... Persbericht lezen
No one enjoys going to the dentist; young children even less so. To help future dentists and dental assistants deal with children during dental treatments, the Japanese company tmsuk has developed a humanoid robot that realistically simulates the behaviour of young children during these treatments, complete with fidgeting, flinching or closing the mouth. The dummy’s realistic movements are produced using proportional pressure regulators with piezo technology from Festo. Persbericht lezen Afbeelding tmsuk, Japan 2023/03/13 | Wereldwijd No longer afraid of the dentist No one enjoys going to the dentist; young children even less so. To help future dentists and dental ... Persbericht lezen
2024/11/07 | Global Compamed 2024 Compamed is the leading exhibition for high-tech solutions in the medical technology sector. Persberichten (9) Afbeeldingen (34) Persmap bekijken Afbeelding Festo SE & Co. KG
2023/11/08 | Global Compamed 2023 Compamed is the leading exhibition for high-tech solutions in the medical technology sector. Persberichten (9) Afbeeldingen (32) Persmap bekijken Afbeelding Festo SE & Co. KG