© Festo SE & Co. KG
Christian Tarragona
„Door de nauwkeurige drukregelaars in de gewrichten van de robot, herkent hij wanneer hij wordt aangeraakt en reageert daarop met de betreffende veiligheidsfuncties”, vult Christian Tarragona, leider Robotics bij Festo aan.
Dutch translation unavailable for Festo and MassRobotics Select Companies for the Inaugural Healthcare Robotics Startup Catalyst Program.
© Festo SE & Co. KG
2023/03/13
|
Wereldwijd
Better gripping with intelligent picking robots
Production, warehouse, shipping - where goods are produced, stored, sorted or packed, picking also takes place. ...
Persbericht lezen
Production, warehouse, shipping - where goods are produced, stored, sorted or packed, picking also takes place. This means that several individual goods are removed from storage units such as boxes or cartons and reassembled. With the FLAIROP (Federated Learning for Robot Picking) project Festo and researchers from the Karlsruhe Institute of Technology (KIT), together with partners from Canada, want to make picking robots smarter using distributed AI ...
Dutch translation unavailable for DAV Tech realizza con Festo stazioni di dosaggio robotizzate.
Dutch translation unavailable for Elettromeccanica Pantanetti integra la tecnologia Festo alla robotica.
© Festo SE & Co. KG
Delta robotics without control cabinet 3
Industry 4.0: the development project can be integrated into a plant as a virtual model.
© Festo SE & Co. KG
Delta robotics without control cabinet 2
Industry 4.0: the development project can be integrated into a plant as a virtual model.
© Festo SE & Co. KG
Delta robotics without control cabinet 1
Delta robotics without control cabinet: a development project from Festo enables this vision.
© Festo SE & Co. KG
Head Office
Head Office of Festo in Esslingen a.N., Germany (Photo: Festo SE & Co. KG)