2020/10/07
|
Ierland, Groot-Brittannië
New VYKA media separated valve range from Festo
Industrial automation specialist Festo has introduced the VYKA range of media separated solenoid valves ...
Persbericht lezen
Industrial automation specialist Festo has introduced the VYKA range of media separated solenoid valves offering high precision control of virtually any fluid or gas. Just 7mm in width and with an orifice size of 1.2mm, the VYKA range has a class leading pressure-to-orifice size ratio and offers a compact solution to a wide variety of dosing and continuous flow applications.
VYKA media separated solenoid valves from Festo
(pictured here with the VAVE connection box) offer a high precision, compact solution to a wide variety of dosing and continuous flow applications.
Dutch translation unavailable for New Festo VMEF/VHEF manual or mechanically actuated valves deliver great precision.
© Festo SE & Co. KG
VAEM valve controller
Small, light, energy efficient, fast, and precise ‒ the VAEM overcomes the challenges found in micro-dispensing liquids.
Dutch translation unavailable for Festo Achieves a Critical Mass of Life Science Automation Products For COVID-19 Diagnostic Equipment.
Dutch translation unavailable for VTOE.
Dutch translation unavailable for EXCM.
Dutch translation unavailable for Festo EHMD.
© Festo SE & Co. KG
2024/01/23
|
Wereldwijd
Reliable gripping without air
The electric standard gripper EHPS from Festo is the electric version of the pneumatic standard gripper DHPS. ...
Persbericht lezen
The electric standard gripper EHPS from Festo is the electric version of the pneumatic standard gripper DHPS. The EHPS can be used wherever pneumatics is not permissible. The concept of the electric standard gripper is based on simplicity and low complexity – all the electronics are integrated in the gripper, which means that an external motor controller is not required.
© Festo SE & Co. KG
EHPS electric standard gripper
The electric parallel gripper variant EHPS-…-LK with integrated memory for various learning functions.