© Festo SE & Co. KG
2024/05/07
|
Wereldwijd
Many functions safe under the roof of VTUX
Festo is now making it even easier for its users: the functions of the classic valve terminals CPV, MPA-L/S and ...
Persbericht lezen
Festo is now making it even easier for its users: the functions of the classic valve terminals CPV, MPA-L/S and VTUG are now available under the umbrella of the convertible valve terminal VTUX. In addition, the AP-I and AP-A communication system creates the ideal platform for digitalized production. This brings flexibility and openness - true to the motto "Open Architecture".
© Festo SE & Co. KG
VTUX
VTUX: The new valve terminal combines the advantages of three classic valve terminals (photo: Festo)
© Festo SE & Co. KG
2023/12/05
|
Wereldwijd
Eichenberger convinces compared to products from the Chinese market
Eichenberger successfully held its own against local Chinese manufacturers in the planning of the new Festo ...
Persbericht lezen
Eichenberger successfully held its own against local Chinese manufacturers in the planning of the new Festo gripper due to outstanding quality (5000% more operational performance in the endurance test), production from a single source, years of expertise and close cooperation throughout the development process from start to finish.   
© Festo SE & Co. KG
Gripper HEPP
Gripper HEPP with spindle from Eichenberger
© Festo SE & Co. KG
2023/11/08
|
Wereldwijd, Duitsland
A mass flow controller that is silent, fast and cost-effective
 For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow ...
Persbericht lezen
 For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow controller from Festo delivers maximum control dynamics and costs significantly less than comparable solutions for the control of air, oxygen and inert gases.
© Festo SE & Co. KG
VEMD proportional flow control valve
The proportional flow control valve VEMD is a mass flow controller that is silent, dynamic and affordable, and thus ideal for use in the life sciences, food production or biotechnology.
© Festo SE & Co. KG
EHMD in laboratory automation
The compact rotary gripper module EHMD from Festo can handle virtually any gripping task in laboratory automation, no matter how small.  
© Festo SE & Co. KG
2024/05/02
|
Wereldwijd
Reliably gripping and turning small parts
The extremely compact rotary gripper module EHMD is the ideal choice in many life science applications where ...
Persbericht lezen
The extremely compact rotary gripper module EHMD is the ideal choice in many life science applications where small objects need to be gripped and turned in confined spaces. For example, it can be used in laboratory automation to open a variety of sample vials with ease. The Z module automatically adjusts to the thread pitches of the caps, eliminating changeover times.
© Festo SE & Co. KG
Rotary gripper module EHMD
The compact rotary gripper module EHMD comes in a fully electric version or with a pneumatic gripper.