© Festo SE & Co. KG 2021/02/01 | Global Precise and robust The essence of any mechanical switching device is an accurate response. That is exactly why it is designed to ... Ler comunicados de imprensa The essence of any mechanical switching device is an accurate response. That is exactly why it is designed to respond with precision. And why it can be installed, without backlash, in just a few steps. The manually and mechanically actuated valves from the VHEF and VMEF series from Festo follow precisely these mechanical principles.
© Festo SE & Co. KG 2020/10/12 | Global Powerful acceleration, gentle cushioning A powerful drive calls for cushioning that extends the operating life of machines. Festo has addressed this ... Ler comunicados de imprensa A powerful drive calls for cushioning that extends the operating life of machines. Festo has addressed this need by equipping the compact drives ADN-S-… with pneumatic end-position cushioning PPS. The design minimises impact in the end positions while at the same time improving reliability thanks to the self-adjusting cushioning. The small sizes are ideal for the electronics industry and small parts assembly.
© Festo SE & Co. KG 2020/10/01 | Global Reliable gripping without air The electric standard gripper EHPS from Festo is the electric version of the pneumatic standard gripper DHPS. ... Ler comunicados de imprensa The electric standard gripper EHPS from Festo is the electric version of the pneumatic standard gripper DHPS. The EHPS can be used wherever pneumatics is not permissible. The concept of the electric standard gripper is based on simplicity and low complexity – all the electronics are integrated in the gripper, which means that an external motor controller is not required.
© Festo SE & Co. KG 2020/09/22 | Global Nereda® technology for space and energy savings The patented Nereda process from Royal HaskoningDHV offers wastewater treatment plants that take up 75% less ... Ler comunicados de imprensa The patented Nereda process from Royal HaskoningDHV offers wastewater treatment plants that take up 75% less space than conventional plants, require just 50% of the energy and are also odour-free, while delivering excellent purification performance. Pneumatic automation technology from Festo ensures reliable and exact process sequences, while experts from Festo provide support with planning the plant.
2021/02/02 | Global Hannover Messe Preview 2021 What will Festo be focusing on in 2021? In addition to digitalisation, individualisation and sustainability ... Comunicados de imprensa (8) Imagens (30) Vídeos (4) Visualizar pasta de imprensa © Festo SE & Co. KG
2020/10/15 | Global Analytica 2020 Comunicados de imprensa (5) Imagens (16) Vídeos (2) Visualizar pasta de imprensa © Festo SE & Co. KG
2020/07/08 | Global Festo Press Conference 2020 Since the Hannover Messe will be launched as a virtual event this year, we have also redesigned our traditional ... Comunicados de imprensa (7) Imagens (25) Vídeos (2) Visualizar pasta de imprensa © Festo SE & Co. KG
2020/02/12 | Global Hannover Messe Preview 2020 Giving an outlook to Hannover Fair in July 2020 Festo presents news about digitalisation, artificial ... Comunicados de imprensa (5) Imagens (15) Vídeos (1) Visualizar pasta de imprensa © Festo SE & Co. KG