2020/06/17
ID: 3520

Mini factories in containers help reduce face mask shortages

Protective masks have been in short supply in these times of coronavirus. An innovative containerised production facility that enables businesses and healthcare organisations to produce their own masks to order could solve the problem. Developed in just six weeks by Mikron with engineering support from Festo, the mini factory uses a scalable system that can produce 50-100 face masks per minute.

“Normally you’d need six months for systems of this size, but this is time we don’t have during the current coronavirus pandemic,” explains Nils Rödel, General Manager of Mikron Berlin. “So, 20 of our designers and fitters spent a week concentrating fully on this project and came up with a 3D model as the basis for this scalable system.”

The project was accelerated by the engineering support provided by Festo. “Even in this period of crisis, the electric and pneumatic components we needed were available quickly. The fact that integrating and commissioning the electric drive solutions in the system as well as connecting them to the Beckhoff PLC was so quick and easy was also helpful,” says Rödel, adding: “The Festo Automation Suite software made integrating and commissioning the CMMT servo drive child’s play, and we were able to quickly make decisions about the correct sizes.”

Mini factory, big benefits

In the modern world, factories are often sited far from the people who actually need the products they manufacture and relay on complex supply and distribution chains – increasingly spanning different continents. This has been precisely the problem during the coronavirus pandemic: when demand skyrocketed, global supply chains were revealed to be less robust than expected – and prone to corruption. When it comes to medical protective equipment, the failure of a delivery can cost human lives. Mikron’s mini factory closes the gap between point of manufacture and point of consumption, eliminates the need for transport and so makes the end product cheaper.

The beauty of Mikron’s system is that it fits in a 20-foot shipping container, which can also act as a clean room. This makes it compact enough to be sited adjacent to a hospital, shopping centre or school. The integrated air-conditioning system with air purification filters means that production is even possible in places with high risk of viral contamination. Depending on the raw materials, the system can operate autonomously for more than two hours. This reduces the number of people required and consequently the risk of infection. So, the mini factory can also produce protective masks in remote areas or even in crisis zones where meeting hygiene standards is more challenging.

In effect, it would be possible to produce two million protective mouth-nose masks each month with just one system. The masks are based on meltblown non-woven fabric which is made up of many layers of fine fibres, and thus filter out even the smallest particles such as bacteria and viruses from the air being breathed in.

Depending on how it is configured, the system can make packs of ten masks or individual ones, shrink-wrapped for cleanliness and in printed bags and boxes if required. “This involves docking an automated packaging station developed by our project partner pi4_robotics GmbH to the scalable system,” says Rödel.

Innovation driven by Festo

Electric and pneumatic components from Festo ensure the reliable transport of the parts or perform clamping tasks at every stage of the process, from the three-layer unwinding station, to the shaping and folding station for the non-woven fabric, on to the ultrasonic sealing station for sealing the edges and finally attaching the ear loops. Festo’s CMMT servo drives and EMMT electric drives are used in the application, since they can be easily connected to PLCs from other manufacturers such as Beckhoff, Siemens and Rockwell.

The pneumatic components installed in the system are from Festo’s core product range, and include the ADN compact cylinder, the DFM guided drive and the DSNU round cylinder. All these components are attractively priced, in stock worldwide and available within 24 hours. The Festo core product range provided the ability to build systems for producing masks reliably within the shortest possible time. The pneumatic drives are actuated by MPA manifold mounted solenoid valves. MS6-SV-E safety valves ensure that safety-critical system components are exhausted and de-energised as quickly as possible in the event of an emergency stop.

Thanks to its international production and sales network, products from Festo are quickly available in 176 countries and enable systems to be built decentrally at locations around the world. This is entirely in keeping with the global open-source approach of the Carola project, which provided the impetus for designing the system.

The face mask production system needed to be as easy to commission as it is to build. “The current travel restrictions make it extremely difficult for commissioning technicians to get to where the systems are to be built,” says Rödel. So Mikron came up with a digitised solution: “We use the HoloLens, which enables commissioning to be done virtually using an interactive 3D projection.”

 

About Festo 
Festo is a leading international supplier of automation technology with a turnover in 2024 of around €3.45 billion. Festo employs over 20,000 people worldwide and is a proven innovator and problem solver in pneumatic and electrical automation, where it is the performance leader. Festo offers around 36,000 pneumatic and electric products in hundreds of thousands of variants for factory and process automation technology, many of which can be tailored to specific customer needs.  Sustainability, reducing its CO2  footprint, digital learning, innovation, performance and speed are the key drivers for the company's future. Festo GB operates as a carbon neutral organisation and uses the PAS 2060 standard externally audited by NQA to validate this claim to customers, employees and other stakeholders.

Festo Industrial Automation's innovative strength is demonstrated through the launch of around 100 new products every year. The company invests over 8.5% of its turnover in R&D, resulting in over 2,600 patents held worldwide. For more information about the company's products and UK / Irish services, please visit: www.festo.com/gb  and www.festo.com/ie

Festo and Industry 4.0 - Festo has engaged with the Industry 4.0 initiative from its inception: as a user, manufacturer and trainer.  As a member of the steering group, the company has taken an active role in defining the core standards such as the RAMI model and the Administration Shell.  Festo Didactic has installed Industry 4.0 Cyber-Physical Factory training hardware systems in many leading universities and training centres. It also provides Industry 4.0 training courses for change managers and practical workshops for employees. Industry 4.0 technologies such as OPC-UA communications are embedded in the latest generation products. For more information, go to www.festo.com/digitalisation
 
Festo Didactic training delivers training for industry – by industry. Combining Festo's industrial heritage with its future-focused manufacturing and engineering expertise to deliver courses for greater productivity and competitiveness. Offering a wide range of open courses, structured development programmes and tailor-made, customer-specific projects on technology and Industry 4.0 and the industry-leading online training suite, Festo LX. Festo also provides state-of-the-art training equipment solutions for industrial companies and educational institutions around the world. Festo Didactic has around 56,000 education customers worldwide. More information on Festo training and consulting services can be found at: www.festo.com/didactic

Festo Bionic Learning Network encapsulates the innovative nature of Festo, raising awareness and attracting talent to the company. Exploring the links between nature and technology opens new areas of innovation and demonstrates complex ideas in a stimulating and enjoyable way. Festo works with an alliance of internal R&D, external educational establishments and specialist companies to advance bionic solutions for automation applications of the future. The objective is to benefit from bionics as a source of inspiration and to realise these in industrial automation. For more information about Festo's Bionic Learning Network, please visit: www.festo.com/bionics

 

Face mask production system pic 1
Fits in a 20-foot shipping container: Mikron’s system for producing 50-100 protective masks a minute.
Face mask_DFM pic 2
Products from Festo’s core range, like the DFM guided drive shown here, enabled the face mask manufacturing system to be built quickly and reliably.
Face mask - CMMT-ST pic 3
Compatible with higher-level controllers from Beckhoff, Siemens or Rockwell: the CMMT servo drive from Festo.

Pessoa de Contacto Global

Downloads

Partilhar comunicados de imprensa