© Festo SE & Co. KG
Dr. Oliver Jung with SDGs
Festo has aligned its Sustainability Strategy with the Sustainable Development Goals (SDGs) of the United Nations, which are relevant for the company, and aims to be climate-neutral at its main locations by the beginning of 2023. In the picture,...
© Festo SE & Co. KG
Festo QANT_3
The algae are fed to the Q.ANT sensor automatically and continuously by special microfluidic components from Festo.
© Festo SE & Co. KG
Festo QANT_2
A major challenge is to accurately determine the amount of biomass. For this, Festo relies on quantum sensor technology from Q.ANT.
© Festo SE & Co. KG
Festo QANT_1
The Festo developer connects the microfluidic pumps to the Q.ANT sensor to supply the algae fluid.
© Festo SE & Co. KG
VTUG
Reliable: The cylinders are controlled by the VTUG valve terminal.
© Festo SE & Co. KG
2022/05/27
|
Global
Poupe 30% de volume
Portugal, este ano o País-Parceiro da Hannover Messe, é o campeão mundial em rolhas de ...
Ler comunicados de imprensa
Portugal, este ano o País-Parceiro da Hannover Messe, é o campeão mundial em rolhas de cortiça: com a maior área de sobreiros, os portugueses também são os maiores exportadores de cortiça do mundo.   Mesmo a cortiça sendo leve, torna-se um material muito volumoso se for embalado de forma ineficiente. Para poupar energia e reduzir as emissões de CO2 durante o transporte, o ...
© Festo SE & Co. KG
DSNU
Robust: the 20 DSNU round cylinders from Festo's core range press the corks together while they are sucked in by the vacuum cups.
© Festo SE & Co. KG
Cork packaging_2
The robot arm sucks in the corks with vacuum suction cups on its gripper and places them in the cartons to save space.
© Festo SE & Co. KG
Cork packaging_1
The robot arm sucks in the corks with vacuum suction cups on its gripper and places them in the cartons to save space.