© ILLIG Maschinenbau GmbH & Co. KG
ILLIG thermoforming system RDF 85
System with adaptive, variable tool interface: the flexibility of the new thermoforming machine RDF 85 from the RedLine product line enables tool systems from market competitors to be installed.
© ILLIG Maschinenbau GmbH & Co. KG
ILLIG thermoformed packaging
One thing ILLIG is particularly proud of is the ILLIG Technology Center: here, the company works with manufacturers of branded goods and packaging from the food and non-food area to test new packaging materials and shapes.
© Festo SE & Co. KG
2022/04/29
|
Global
On the safe side
With the tubing PUN-H-F and the stainless-steel push-in fitting NPQR, manufacturers of food and packaging ...
Ler comunicados de imprensa
With the tubing PUN-H-F and the stainless-steel push-in fitting NPQR, manufacturers of food and packaging machines are on the safe side. This product combination from Festo guarantees compliance with food safety requirements. But Festo has suitable tubing/fitting combinations for other extreme situations too.
© Festo SE & Co. KG
Tubing PUN-H-F with push-in fitting NPQR
On the safe side: The combination of the tubing PUN-H-F and the stainless-steel push-in fitting NPQR from Festo guarantees compliance with food safety requirements for manufacturers of food and packaging machines.
© Festo SE & Co. KG
Tubing PUN-H-F
Tubing PUN-H-F: For highly versatile use in food applications, the “natural” colour variant can also be used in applications with gaseous oxygen.
© Festo SE & Co. KG
SDBT Cylinder sensor
Faster assembly times and more reliable cylinder switching are two advantages of the latest pneumatic innovation from Festo.
© Festo SE & Co. KG
Screenshot GUI of pressure and vacuum generator PGVA
Simple: with a PC and the GUI software, the necessary parameters can be transferred via the COM or Ethernet port.
© Festo SE & Co. KG
PGVA pressure and vacuum generator, interior view
Integrated: compressor, filter system, reservoirs and electronic pressure/vacuum control with proportional regulator.