© Festo SE & Co. KG
CMSH positioner on quarter turn actuator with VTOP
Easy and safe installation of the CMSH on the actuator with VTOP with integrated air supply to VDE/VDI 3847-2. This eliminates the need for external piping and significantly reduces the susceptibility to leakages.
PCE Stanley knives - assembly
A combination of Festo DGST mini-slides, axes, cylinders and grippers are used to pick and place the STANLEY knife components with high precision and repeatability.
© Festo SE & Co. KG
PCE Stanley Knives - CPX-API automation platform
© Festo SE & Co. KG
2021/05/25
|
Global
The fast way to a safe insulin pen
Diabetes is on the rise worldwide with around 10 million people being diagnosed with the disease every year. ...
Ler comunicados de imprensa
Diabetes is on the rise worldwide with around 10 million people being diagnosed with the disease every year. This pushes up the demand for insulin pens for self-injection. Syntegon's Danish subsidiary has developed an automated system for assembling these pens using the Festo automation platform.
© Syntegon
Ulrik Keldke, Syntegon
Ulrik Keldke, Head of Syntegon's engineering department in Sandved: "What we appreciate about the Festo servo press kit is the ease of commissioning." (Photo: Syntegon)
© Syntegon
Michael Andersen, Syntegon
Michael Andersen, Sales Director of Syntegon Technology Sandved in Denmark: "The servo press kit from Festo supports us in the 'flying format change' project." (Photo: Syntegon)
© Syntegon
Festo automation at Syntegon line
Automation with pneumatics and electrics ensures safe and reliable processes so that the end product, the insulin pen, can also be safe and user-friendly (Photo: Syntegon)
© Syntegon
Servo Press Kit YJKP at Syntegon
The servo press kit YJKP performs three joining and pressing steps: from inserting the cartridge, needle and spring to inserting the glass and plastic covers (Photo: Syntegon)  
© Syntegon
Syntegon assembly line for insulin pens
General view of the new machine: Syntegon's automatic assembly lines produce up to 300 insulin pens per minute, depending on the model. The degree of automation is scalable according to requirements and can also be adapted at a...