© Festo SE & Co. KG
Festo QANT_2
A major challenge is to accurately determine the amount of biomass. For this, Festo relies on quantum sensor technology from Q.ANT.
© Festo SE & Co. KG
Festo QANT_1
The Festo developer connects the microfluidic pumps to the Q.ANT sensor to supply the algae fluid.
© Festo SE & Co. KG
VTUG
Reliable: The cylinders are controlled by the VTUG valve terminal.
© Festo SE & Co. KG
2022/05/27
|
全球
Save 30 per cent volume
Portugal is the cork world champion: with the largest acreage under cork oaks, the Portuguese are also the ...
阅读新闻稿
Portugal is the cork world champion: with the largest acreage under cork oaks, the Portuguese are also the largest cork exporters worldwide. Although cork itself is light, it is all the more voluminous if it is packaged inefficiently. In order to save energy and CO₂ emissions during transport, the ESI Group developed a system for packaging corks that requires 30 per cent less packaging volume and does without plastic. On board: automation ...
© Festo SE & Co. KG
DSNU
Robust: the 20 DSNU round cylinders from Festo's core range press the corks together while they are sucked in by the vacuum cups.
© Festo SE & Co. KG
Cork packaging_2
The robot arm sucks in the corks with vacuum suction cups on its gripper and places them in the cartons to save space.
© Festo SE & Co. KG
Cork packaging_1
The robot arm sucks in the corks with vacuum suction cups on its gripper and places them in the cartons to save space.
© Festo SE & Co. KG
PhotoBionicCell_CPX
Automation system CPX-E: Controls all processes in the tank and communicates with the cloud
© Festo SE & Co. KG
PhotoBionicCell_Valve
Valve sensor unit for controlling the circulation in the surface collectors
© Festo SE & Co. KG
PhotoBionicCell_Q.ANT
Quantum sensor: Optical real-time determination of biomass