© Festo SE & Co. KG
SupraMotor_3
The SupraMotor has a high overload capacity and is suitable for applications in continuous operation.
© Festo SE & Co. KG
SupraMotor_2
The SupraMotor only needs energy for cooling in the low three-digit watt range.
© Festo SE & Co. KG
SupraMotor_1
Superconducting compact claw pole motor with electrical solid-state cooling.
© Festo SE & Co. KG
Bionics4Education_4
Bionics Kits for creative minds: Discovering the fascinating world of bionics in a playful way, and learning about technology with fun and enjoyment.
© Festo SE & Co. KG
Bionics4Education_3
Education in the digital era: Intuitive control of the robotic animals by smartphone or tablet.
© Festo SE & Co. KG
Bionics4Education_2
Three robotic models can be generated from the one kit – ideal for multidisciplinary teaching at schools.
© Festo SE & Co. KG
Bionics4Education_1
Bionics4Education: An integral didactic concept comprising learning kits and a digital learning environment.
© Festo SE & Co. KG
2023/01/13
|
全球
Unique forms of motion derived from nature
Walking and rolling like the flic-flac spider – the BionicWheelBot moves along the ground in astounding ...
阅读新闻稿
Walking and rolling like the flic-flac spider – the BionicWheelBot moves along the ground in astounding ways. Together with the team headed by the discoverer of the spider, Professor Ingo Rechenberg, Festo has taken a very close look at these unique forms of locomotion and has technically realised them. But no magnifying glass was needed for the flying fox: the BionicFlyingFox is an imposing figure with its wingspan of 2.28 metres and its partly ...
© Festo SE & Co. KG
BionicFlyingFox 2
The wing kinematics of the BionicFlyingFox are also divided into primaries and secondaries.
© Festo SE & Co. KG
BionicFlyingFox 1
Despite its wingspan of 228 cm and its overall length of 87 cm, the BionicFlyingFox weighs 580 grams.