© Festo SE & Co. KG
2020/07/30
|
全球
The right handling system in just 20 minutes
As of immediately, technicians and engineers arrive at the right ready-to-install handling system at a ...
阅读新闻稿
As of immediately, technicians and engineers arrive at the right ready-to-install handling system at a record-breaking tempo in the areas of project engineering and planning. They can now order new system solutions intelligently and intuitively via the new Festo Handling Guide Online – without any interruptions in the value chain because the new configuration and ordering platform is integrated into the online product catalogue from Festo.
© Festo SE & Co. KG
Handling
With the Handling Guide Online, machine and equipment manufacturers are able to reduce time-to-market by the revolutionary amount of roughly 70% with regard to integrated handling systems.
© Festo SE & Co. KG
Handling Guide Online Screen 3 EN
Selected handling system in the Handling Guide Online: the data sheet and the correctly configurated CAD model are immediately made available for download in all common data formats.
© Festo SE & Co. KG
Handling Guide Online Screen 2 EN
Structured data querying and planning security: a large portion of the engineering costs are eliminated and detailed product knowledge is unnecessary.
© Festo SE & Co. KG
Handling Guide Online Screen 1 EN
Handling Guide Online from Festo: allows design and project engineers to configure and order new system solutions intelligently and intuitively – in just 20 minutes.
© Festo SE & Co. KG
Actuators with decentralised control units
Having the positioner function in a decentralised control unit, in other words not directly at or in the actuator, opens up new horizons right up to the use of artificial intelligence.
© Festo SE & Co. KG
VTUG
Quickly connected to all commonly available fieldbuses: the valve terminal VTUG plug-in, as a new family member of the VG series, is electrically modular and pneumatically flexible - also in the control cabinet.
© Festo SE & Co. KG
Electronics manufacturing testing
Electronics manufacturing at the Scharnhausen Technology Plant: Different testing methods ensure high quality. These range from automatic optical inspection (AOI) through in-circuit tests (ICT) to system tests (EOL test).
© Festo SE & Co. KG
Electronics manufacturing SMD devices
Electronics manufacturing at the Scharnhausen Technology Plant: Tens of thousands of units of the CPX are assembled according to customer requirements every year. This requires up to 300 different components, including electronic components such...
© Festo SE & Co. KG
Delta robotics without control cabinet 3
Industry 4.0: the development project can be integrated into a plant as a virtual model.