© Festo SE & Co. KG
Fast MDx - operator
After manual placement, operators can focus on their actual task, namely analysing the results.
© Festo SE & Co. KG
Fast MDx - gripping
Fully automated tests: a separate handling system, based on the EXCM-30 planar surface gantry, uses electric griper EHPS-16 to transport and position the microwell plate between the individual processing steps.
© Festo SE & Co. KG
Fast MDx - pipetting 2
The automated pipetting system, consisting of the pipetting head DHOE from Festo and the disposable syringe ejector DHAO, can accurately dispense volumes in the range of 10 µl.
© Festo SE & Co. KG
Fast MDx - pipetting 1
Space-saving: one gantry each takes care of pipetting and dispensing liquids as well as transporting and positioning the microwell plate.
© Festo SE & Co. KG
Fast MDx - testing system
High throughput: two 3D gantries with pipetting and transport units ensure a fully automated sequence of molecular diagnostic tests.
© Festo SE & Co. KG
Three-dimensional gantry EXCL
The three-dimensional gantry EXCL can accommodate two independent Z-axes, with a rotary gripper for opening and closing on the right and a pipetting system for aspirating and dispensing on the left.
© Festo SE & Co. KG
Aspirating
Fast and reliable aspiration: the dispense head VTOI controls all eight channels with just one valve.
© Festo SE & Co. KG
Dispensing
Dispensing various liquids and filling quantities: the dispense head VTOE from Festo offers a wide range of possible applications.  
© Festo SE & Co. KG
Pipetting
Reliable pipetting results: intelligent pipette head DHOP set up with the finely tuned disposable tips DHAP.
© Festo SE & Co. KG
2022/06/15
|
全球
Smart pipetting for safe laboratory processes
Handling the smallest amounts of liquids down to the microlitre range requires high levels of precision and ...
阅读新闻稿
Handling the smallest amounts of liquids down to the microlitre range requires high levels of precision and flexibility because of the changing fluid properties of the different media. Pressure-controlled liquid handling systems enable precise, scalable liquid handling. Festo has suitable solutions for these systems, whether for pipetting, dispensing or aspirating. Individual modules are available, such as the smart pipette head DHOP, but as well the ...