© Festo SE & Co. KG
MolGen - Pipetting
Extremely small pipetting volumes: the second robot arm with the pipetting head distributes liquids onto a microwell plate.
© Festo SE & Co. KG
MolGen - Opening vial
During the initial work operation, the first robot arm grasps a sample vial by the cap with an electric gripper and brings it into a position at which the cap is removed.
© Festo SE & Co. KG
MolGen - Gripping vial
During the initial work operation, the first robot arm grasps a sample vial by the cap with an electric gripper and brings it into a position at which the cap is removed.
© Festo SE & Co. KG
MolGen - PurePrep TTR
High throughput: the fully automated PurePrep TTR system prepares 320 patient samples per hour for PCR testing. Laboratory-specific automation technology from Festo is included.
Chinese, Simplified translation unavailable for The New Festo Solution for DeltaV DCS Expands Integration Options and Productivity.
Fast MDx 4
Fully automated tests: a separate Festo handling system uses the EHPS-16 electric gripper to transport and position the microwell plate between the individual processing steps.
Fast MDx 3
The automated pipetting system, consisting of the DHOE pipetting head and the DHAO disposable syringe ejector from Festo, can accurately dispense volumes in the range of 10 µl.
Fast MDx 2
High throughput: two Festo 3D gantries with pipetting and transport units ensure a fully automated sequence of molecular diagnostic tests in the Fast MDx.
Fast MDx 1
Richard Lewis, founder and CEO of Fast MDx.