© Festo SE & Co. KG
ELCC cantilever axis
ELCC cantilever axis from Festo can cut cycle times in handling applications by up to 30%.
DFPC pneumatic linear actuator
Freedom of choice: The double-acting pneumatic linear actuator DFPC from Festo for process valves is available either as low-cost, preconfigured standard variants from stock or as individually configured versions.
© Festo SE & Co. KG
2020/04/09
|
全球
Chameleon’s tongue for industrial automation wins design prizes
Grasping workpieces like a chameleon’s tongue – that’s the functional principle of ...
阅读新闻稿
Grasping workpieces like a chameleon’s tongue – that’s the functional principle of Festo’s adaptive shape gripper DHEF. The gripper can thus pick, gather and place objects of many different shapes without any need for manual changeovers. This is why it won renowned distinctions in 2020 including the iF Design Award and the Red Dot Design Award.
© Festo SE & Co. KG
DHEF Adaptive Shape Gripper 1
Adaptive shape gripper DHEF: like a chameleon’s tongue, it reliably grasps irregular, round and sensitive objects. Festo’s gripper won the internationally acclaimed iF Design Award and Red Dot Design Award for this extraordinary gripping concept.
© Festo SE & Co. KG
Cabinet Guide Online 2
Numerous custom control cabinet variations possible with the online tool Cabinet Guide Online. (Image: Festo SE & Co. KG)
© Festo SE & Co. KG
Cabinet Guide Online 1
A custom control cabinet in record time with the online tool Cabinet Guide Online.
Chinese, Simplified translation unavailable for VAEM.
© Festo SE & Co. KG
VEAE in ventilator breathing devices
The proportional valve VEAE is suitable for portable or stationary ventilator breathing devices for outpatient or hospital use.
© Festo SE & Co. KG
VEAE proportional valve
The proportional valve VEAE from Festo reliably and precisely regulates gas flows, whether oxygen, air, nitrogen or inert gases.
Supra Drive 2.0
© Festo SE & Co. KG
SupraDrive 2.0
With superconductor technology, objects can be stored and moved without contact – as with the SupraDrive 2.0.