Gearbox SMS image 3
De tijdspanne tussen beoordeling door de AI en de beslissing goed- of afkeur, slechts 0,3 seconde.
Gearbox SMS image 2
Het controleproces start met punnets met druiven die via een transportband in de machine onder de camera door worden gevoerd.
Gearbox SMS image 1
Druivencontrole versneld door vision, AI en SMS
© Festo SE & Co. KG
Gerhard Borho
Member of the Management Board Information Technology and Digitalisation, Festo SE & Co. KG
© Festo SE & Co. KG
Digital twin handling portal
Designing and programming efficient handling systems using the virtual model: That is how errors can be detected and corrected at an early stage, which significantly contributes to efficient and stable operation later on.
© Festo SE & Co. KG
Graphic digital twin (cube)
Faster time-to-market, more efficient engineering, more functionality and higher quality – these are the benefits of a digital twin for machine and system builders.
© Festo SE & Co. KG
BionicCellFactory Algae
The alge is filled into the BionicCellFactory.
© Festo SE & Co. KG
BionicCellFactory User
With automation technology from Festo, biomass can be cultivated on a large scale in a highly efficient, resource-conserving way.
© Festo SE & Co. KG
BionicCellFactory CPX
Control architecture: each module is controlled by a CPX-E controller from Festo.
© Festo SE & Co. KG
BionicCellFactory
The BionicCellFactory factory is divided into five modules in which nature and technology coalesce in different ways.