2022/06/15
ID: 2530

Ready-to-install solutions for the lab-on-a-chip

Automation and engineering for in vitro diagnostics

In medical practices, mobile analytical devices featuring "lab-on-a-chip" technology enable fast testing to identify pathogens in the case of bacterial or viral diseases. In order to lighten the load of manufacturers of these devices for in vitro diagnostics, Festo offers ready-to-install automation solutions, including customer-specific engineering.

A range of suitable miniature cylinders, valves and sensors is available from Festo for bench-top units used to conduct medical analyses on postcard-sized cartridges (lab-on-a-chip). Even more important, however, are ready-to-install customised solutions, which Festo develops in collaborative engineering projects with customers.

 

Focus on core competencies

The ready-to-install solutions are compact, space-saving modules that have clear interfaces for easy integration and therefore offer reduced time to market for customers. Manufacturers and developers of such bench-top units can therefore concentrate on their core competencies. To automate the analysis processes on postcard-sized cartridges, they can rely on the many years of automation expertise of the engineers and developers at Festo.

 

In addition to channels and reservoirs for chemicals, the cartridges contain an area for applying a drop from a blood sample, for example. The analysis process starts when the cartridge is inserted into the device. Miniature cylinders use compressed air to activate the reservoirs with the chemicals. The membranes are pressed down on the cartridges, and the chemicals make their way through the channels at the right time (using capillary forces) to react with the blood. The analysis results are read out at the end of the multi-stage analysis process.

 

Complete automation portfolio

The miniature cylinders EG and EGZ provide the actuator technology for the smallest of spaces. The miniature valves VOVK, MHA1, VEMC and VEMP can control large numbers of tightly packed channels. Miniature sensors SPTE are used for pressure monitoring. The proportional-pressure regulators VEAB with piezo technology round off the automation portfolio from Festo for in vitro diagnostics.

Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,600 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.65 billion in 2023. Each year around 7% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.

© Festo SE & Co. KG
Festo LifeTech
Mobile analytical devices allow fast testing to identify pathogens in the case of colds or flu-like infections as well as other bacterial or viral diseases.
© Festo SE & Co. KG
Valve block for the point-of-care application
Based on the layout of the microfluidic chip, Festo develops the appropriate valve block for the point-of-care application.
© Festo SE & Co. KG
Miniature valve VOVK
Compact components: The miniature valves VOVK activate the process which ensures that the liquid reagents react with each other and the analysis process starts.