Condition monitoring in the cloud at the press of a button
Detecting irregularities at an early stage and initiating the necessary measures before a system failure – this is now made possible by the dashboards and IoT gateway CPX-IOT from Festo. The turnkey, preconfigured dashboards from Festo do not need any additional programming or installation of software. The collected data improves operating transparency for production managers and operators.
Further processing and long-term analysis of data takes place in the cloud. Festo dashboards visualise the information gathered. Festo thus supports machine builders and end users in several steps – through the visualisation and processing of data. The result is increased productivity through better utilisation (overall equipment effectiveness (OEE)), lower costs due to greater energy efficiency and fewer downtimes thanks to comprehensive diagnostics, condition monitoring and improved maintenance. System operators can compare the process control systems of their machines across several locations and identify potential for saving energy. The data can be called up at any time.
Key components for the Internet of Things
The IoT gateway CPX-IOT – the hardware for unlimited communication – connects components and modules from the field level, such as the valve terminal CPX/MPA, the energy monitoring module MSE6-E2M or handling systems, to the Festo Cloud through the OPC UA interface. CPX-IOT collects information and data on Festo devices and their statuses through an Ethernet-based interface and a standardised communication protocol, such as OPC UA. It then sends that information to the cloud through the second Ethernet connection using IoT protocols. The preconfigured dashboard visualises the appropriate information and spares users tiresome programming work. Suitable IT security mechanisms ensure data security in the process.
Breakthrough in digitalisation
With Festo dashboards, Festo is driving digitalisation forward and supporting its customers to enter the digital age. Automation expert Festo is combining its extensive knowledge of industrial applications with the latest developments in information technology to realise online applications for industrial automation practice. Festo is also using digital communication to support its customers throughout the Digital Customer Journey. This digital journey guides customers reliably and comprehensively through the Festo portfolio, from information procurement and configuration through ordering and delivery to commissioning and maintenance or even the technical training offering of Festo Didactic.
Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,800 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.81 billion in 2022. Each year around 7% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.