Condition monitoring in the cloud at the press of a button
Detecting irregularities at an early stage and initiating the necessary measures before a system failure – this is now made possible by the dashboards and IoT gateway CPX-IOT from Festo. The turnkey, preconfigured dashboards from Festo do not need any additional programming or installation of software. The collected data improves operating transparency for production managers and operators.
Further processing and long-term analysis of data takes place in the cloud. Festo dashboards visualise the information gathered. Festo thus supports machine builders and end users in several steps – through the visualisation and processing of data. The result is increased productivity through better utilisation (overall equipment effectiveness (OEE)), lower costs due to greater energy efficiency and fewer downtimes thanks to comprehensive diagnostics, condition monitoring and improved maintenance. System operators can compare the process control systems of their machines across several locations and identify potential for saving energy. The data can be called up at any time.
Key components for the Internet of Things
The IoT gateway CPX-IOT – the hardware for unlimited communication – connects components and modules from the field level, such as the valve terminal CPX/MPA, the energy monitoring module MSE6-E2M or handling systems, to the Festo Cloud through the OPC UA interface. CPX-IOT collects information and data on Festo devices and their statuses through an Ethernet-based interface and a standardised communication protocol, such as OPC UA. It then sends that information to the cloud through the second Ethernet connection using IoT protocols. The preconfigured dashboard visualises the appropriate information and spares users tiresome programming work. Suitable IT security mechanisms ensure data security in the process.
Breakthrough in digitalisation
With Festo dashboards, Festo is driving digitalisation forward and supporting its customers to enter the digital age. Automation expert Festo is combining its extensive knowledge of industrial applications with the latest developments in information technology to realise online applications for industrial automation practice. Festo is also using digital communication to support its customers throughout the Digital Customer Journey. This digital journey guides customers reliably and comprehensively through the Festo portfolio, from information procurement and configuration through ordering and delivery to commissioning and maintenance or even the technical training offering of Festo Didactic.
Festo è un attore globale e un'azienda indipendente a conduzione familiare con sede a Esslingen am Neckar, in Germania. Fin dagli inizi Festo ha stabilito degli standard nella tecnologia dell'automazione industriale e nella formazione tecnica, contribuendo così allo sviluppo sostenibile dell'ambiente, dell'economia e della società. Prodotti e servizi sono disponibili in 176 paesi del mondo. L'azienda, infatti, fornisce tecnologia di automazione pneumatica ed elettrica a 300.000 clienti di automazione di fabbrica e di processo in oltre 35 industrie. Il settore LifeTech con la tecnologia medica e l'automazione di laboratorio sta diventando sempre più importante. Con circa 20.800 dipendenti in oltre 250 filiali in circa 60 paesi in tutto il mondo, Festo ha realizzato un fatturato di circa 3,81 miliardi di euro nel 2022. Ogni anno circa il 7% di questo fatturato viene investito in ricerca e sviluppo, mentre l'1,5 % del fatturato è investito nella formazione di base e di perfezionamento. Festo Didactic SE è un fornitore leader di formazione e formazione tecnica e offre ai suoi clienti in tutto il mondo soluzioni complete di apprendimento digitale e fisico in ambiente industriale.