Multifunctional in the smallest of spaces
The decentralised pressure and vacuum generator PGVA from Festo is a compact complete solution for laboratory automation. It integrates compressor, air preparation including filter system, reservoir and electronic pressure and vacuum control in the smallest of spaces.
Whether your laboratory processes involve pipetting medical samples or dosing with a dispense head, the pressure and vacuum generator PGVA from Festo is a standalone solution for liquid handling in laboratory automation. All you need to supply a solution with compressed air or vacuum is a 24 V power supply.
Practical interfaces
Both pressure and vacuum are generated in a closed control loop using integrated compressor, buffer reservoirs, pressure sensors and proportional valve. Users can individually specify the pressure and vacuum level via a serial RS232 or network-capable Ethernet communication interface. The defined electric, pneumatic and software-based interfaces make it easy to integrate the PGVA into an existing liquid handling solution or operate it manually with the PC-based graphical user interface (GUI). The required volume for dispensing or aspirating is determined by the valve opening time and the pressure and vacuum values set in the software.
Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. The LifeTech sector with medical technology and laboratory automation is becoming increasingly important. The products and services are available in 176 countries. With about 20,000 employees in over 250 branch offices in 61 countries worldwide, Festo achieved a turnover of around €2.84 billion in 2020. Each year around 8 % of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.