Added value from data reduces downtime and waste
On the shopfloor, machines not only deliver products, but also large amounts of data that are converted into ...
Leer nota de prensa
On the shopfloor, machines not only deliver products, but also large amounts of data that are converted into information using artificial intelligence in such a way that they show humans specific optimization potential . Initial successes are visible: in hundreds of customer applications, solutions from the Festo AX Industrial Intelligence portfolio have reduced unplanned downtimes by up to 25 % and cut waste by 20 %.