With the blister packaging machine from IWK, sustainability is not just lip service: with recyclable packaging material, low energy consumption, high speed and ergonomics, the CABLIblue 870 card-to-card blister system is proving to be a real trendsetter. The use of electrical automation technology from Festo increases sustainability and efficiency immensely in this application. Read press release Image Festo SE & Co. KG 04/24/2026 | Global How packaging machines are becoming more ... With the blister packaging machine from IWK, sustainability is not just lip service: with recyclable ... Read press release
Festo, one of the world's leading manufacturers of automation technology, is fully integrating Eichenberger Gewinde AG from Burg in Switzerland as of April 1, 2026. In future, the Swiss company will operate under the name "Festo Gewindetriebe AG". Read press release Image Festo SE & Co. KG 03/31/2026 | Global Eichenberger becomes Festo Festo, one of the world's leading manufacturers of automation technology, is fully integrating ... Read press release
Innovative guide technology, high rigidity and guide load capacity for more load in the same installation space - these are the features of the new ELGD axis family from Festo. In addition, powerful drive elements offer high feed forces and accelerations for shorter cycle times and a long service life. A stainless steel cover strip is friction-free on the outside and does not allow any particles to form there. This makes the drives in the axis family ideal for use in cleanrooms. Read press release Image Festo SE & Co. KG 11/24/2025 | Global Precise and dynamic Innovative guide technology, high rigidity and guide load capacity for more load in the same ... Read press release
Innovative guide technology, high rigidity and guide load capacity for more load in the same installation space - these are the features of the new ELGD axis family from Festo. In addition, powerful drive elements offer high feed forces and accelerations for shorter cycle times, a long service life and less downtime. A stainless steel cover strip is friction-free on the outside and does not allow any particles to form there. This makes the drives in the axis family ideal for use in cleanrooms. Read press release Image Festo SE & Co. KG 2024/11/07 | Global Precise and dynamic Innovative guide technology, high rigidity and guide load capacity for more load in the same ... Read press release
11/23/2025 | Global SPS 2025 The automation trade fair in Nuremberg Press Releases (5) Images (9) View press kit Image Arturo Rivas
2025/02/10 | Global LogiMAT March 11 - 13, 2025. Stuttgart Trade Fair Centre. You are cordially invited to visit the Festo Booth in hall 3, stand ... Press Releases (4) Images (10) View press kit Image Festo SE & Co. KG
2024/11/07 | Global SPS 2024 - The Automation Summit in Nuremberg from ... The SPS from 12 – 14 November 2024 in Nuremberg is the industry highlight of the automation sector and, with its large ... Press Releases (7) Images (11) View press kit Image Festo SE & Co. KG