The manual dismantling of end-of-life batteries in electric vehicles is now a thing of the past: Liebherr has developed a system that automatically removes the battery cover screws - regardless of whether they are attached horizontally or vertically to the battery housing. The CMAD servo-pneumatic position controller from Festo, which makes position-independent unscrewing possible in the first place, plays a major role in this automation solution. Lire le communiqué de presse Image Festo SE & Co. KG 2026/05/29 | Global Automated dismantling of electric batteries The manual dismantling of end-of-life batteries in electric vehicles is now a thing of the past ... Lire le communiqué de presse
Experts estimate that around 3 million tonnes of used batteries from electric cars will be due for recycling in 2030. This inevitably raises the question of sustainability, as batteries are energy storage devices made from critical raw materials. Festo therefore not only offers modular automation concepts for cell production, the assembly of battery modules and packs and for platform integration, but also for dismantling and recycling or separating the materials. Lire le communiqué de presse Image Festo SE & Co. KG 2026/05/29 | Global Automated processes for battery recycling Experts estimate that around 3 million tonnes of used batteries from electric cars will be due for ... Lire le communiqué de presse
Avec la machine de conditionnement sous blister d'IWK, la durabilité n'est pas un vain mot : avec un matériau d'emballage recyclable, une faible consommation d'énergie, une vitesse élevée et une grande ergonomie, le système de conditionnement sous blister Card-to-Card CABLIblue 870 s'avère être un véritable créateur de tendances. L'utilisation de la technique d'automatisation électrique de Festo augmente immensément la durabilité et l'efficacité dans cette application. Lire le communiqué de presse Image Festo SE & Co. KG 24.04.2026 | Globale Comment les machines d'emballage deviennent plus ... Avec la machine de conditionnement sous blister d'IWK, la durabilité n'est pas un vain mot : avec un ... Lire le communiqué de presse
Hydrogen makes sustainable energy mobile. With the intel ligent trailer control system HY.Runner from GP Joule, transporting hydrogen is more efficient, safer, and more environmentally friendly. The Festo valve terminal VTUG and the solenoid valve VOFC provide a space-saving design on the trailer chassis, as well as additional safety. Lire le communiqué de presse Image Festo SE & Co. KG 2025/10/15 | Globale Sustainable, smart, safe Hydrogen makes sustainable energy mobile. With the intel ligent trailer control system HY.Runner ... Lire le communiqué de presse
29.05.2026 | Globale The Battery Show Europe 2026 Visitez Festo au salon de Stuttgart, hall 3, stand E10 Communiqués de presse (4) Images (16) Voir le dossier de presse Image Festo SE & Co. KG
2024/05/28 | Global Battery Show Europe 2024 Reliable, economical, sustainable: The circular battery life cycle – solutions from cell production right up to ... Communiqués de presse (4) Images (15) Voir le dossier de presse Image Festo SE & Co. KG
22.05.2023 | Global Battery Show Europe 2023 Fiable, économique, durable : Le cycle de vie circulaire des batteries - des solutions de la production des cellules ... Communiqués de presse (5) Images (17) Voir le dossier de presse Image Festo SE & Co. KG
2023/02/14 | Global Hannover Messe Press Preview 2023 The future of our planet also presents Festo with major challenges. On the one hand, it is about supplying the world's ... Communiqués de presse (4) Images (23) Voir le dossier de presse Image Festo SE & Co. KG