© WorldSkills International
Industry 4.0
The new skill in Shanghai is Industry 4.0.
© Festo SE & Co. KG
2021/08/31
|
Globale
Safety in fail-safe mode
The preconfigured fail-safe circuit in the ready-to-install control cabinet is a safe and low-cost alternative ...
Lire le communiqué de presse
The preconfigured fail-safe circuit in the ready-to-install control cabinet is a safe and low-cost alternative when it comes to fail-safe technology. It replaces a single-acting actuator and guarantees that the actuator assumes a predefined safety position in the event of a pressure and/or power failure.
© Festo SE & Co. KG
Control cabinet with fail-safe circuit
Safe and low-cost: the preconfigured fail-safe circuit in the ready-to-install control cabinet. 
© Festo SE & Co. KG
2022/05/23
|
Globale
Servo-pneumatic welding guns from Festo reduce downtimes by 25 percent
A leading car manufacturer has been relying on the pinpoint accuracy and efficiency of servo-pneumatic welding ...
Lire le communiqué de presse
A leading car manufacturer has been relying on the pinpoint accuracy and efficiency of servo-pneumatic welding guns from Festo for many years. So much so that they have now installed more than 2,500 welding gun robots with this technology in the premium brand’s body shops. This car manufacturer has now been able to reduce downtimes by 25 percent thanks to a predictive maintenance system from Festo which is ready for artificial intelligence.
© Festo SE & Co. KG
Dashboard Predictive Maintenance
Everything in sight: dashboards for predictive maintenance offer an overview of the machine status.
French translation unavailable for Soluzioni integrate per la gestione dei liquidi.
French translation unavailable for Erweiterung des Official Partner Netzwerkes.
© Festo SE & Co. KG
Pneumatic drives from core range
Impressive value for money: the compact pneumatic drives ADN-S, DSNU and DGST are part of the Festo core product range, which means fast delivery even in large quantities. 
© Festo SE & Co. KG
2021/07/05
|
Globale
Robuste et polyvalent
Les actionneurs pneumatiques de la gamme standard Festo permettent de répondre à une demande ...
Lire le communiqué de presse
Les actionneurs pneumatiques de la gamme standard Festo permettent de répondre à une demande élevée, d'offrir un excellent rapport coût/performance, et ce, toujours avec la haute qualité Festo habituelle pour chaque fonction. Du vérin compact ADN-S au vérin cylindrique DSNU ou au mini chariot DGST, ces actionneurs résolvent les tâches de mouvement requises dans la plupart des ...
© Festo SE & Co. KG
Mini-chariot DGST
Rapport coût/performance impressionnant : le mini chariot DGST fait partie de la gamme de produits stanard Festo, ce qui signifie une livraison rapide même en grande quantité.