© Festo SE & Co. KG
Actionneur quart de tour DFPD
Polyvalent, robuste et conçu pour les extrêmes - le nouvel actionneur quart de tour DFPD pour une utilisation dans l'automatisation de process.
© Festo SE & Co. KG
Support
Competent advice: experts from Festo are available to help with the calculation of the compressed air consumption and the optimum layout of the compressed air network, and can also provide support during the tendering process on request.
© Festo SE & Co. KG
Safety
Safety first: pneumatic actuators are ideal for use in ATEX zones.
© Festo SE & Co. KG
Water treatment plant Langenau
Cost benefits of pneumatic systems: Pneumatic actuators only require electricity for regulating and generating compressed air; the movement itself is triggered by the compressed air. By contrast, electric actuators continuously need energy for the...
© Festo SE & Co. KG
MSE6-E2M
Saving energy is easy: with its integrated flow rate and pressure sensors, the energy-efficiency module MSE6-E2M automatically reduces and monitors the air consumption of systems.
© Festo SE & Co. KG
Schematic Solution 2
Festo has been offering support for the Eplan circuit diagram software in the form of macros for many years. The new “Schematic Solution” service is another step towards digitalisation.
© Festo SE & Co. KG
Schematic Solution 1
Electropneumatic circuit diagrams for individually configured products such as valve terminals can now be generated fully automatically for the Eplan circuit diagram software.
© Festo SE & Co. KG
SupraMotor_3
The SupraMotor has a high overload capacity and is suitable for applications in continuous operation.
© Festo SE & Co. KG
SupraMotor_2
The SupraMotor only needs energy for cooling in the low three-digit watt range.
© Festo SE & Co. KG
SupraMotor_1
Superconducting compact claw pole motor with electrical solid-state cooling.