2024/02/20
|
Belgique, Irlande, Pays-Bas, Grande-Bretagne
Festo electric drive automation at Mondelez
Mondelez has chosen Festo electric drive technology for a new automated chocolate Easter egg mixing ...
Lire le communiqué de presse
Mondelez has chosen Festo electric drive technology for a new automated chocolate Easter egg mixing installation at its site in Herentals, Belgium. The egg mixing line uses an ingenious system of conveyors to ensure that everyone finds a nice mix of flavours in their pack of chocolate eggs at Easter. Electric drives were chosen over pneumatics because they offer lower energy consumption, higher safety and more flexibility in controlling speeds and ...
Mondelez_Image 3
Thanks to Festo electric drives, a variety of flavour mixes can be achieved without difficulty.
Mondelez_Image 2
Dual Festo ELGA timing belt shafts and ESBF electric cylinders direct the filling conveyor in the correct direction to fill the pallet bins evenly.
Mondelez_Image 1
Bob Aerts (Engineering Mondelez) together with Johan De Pauw (Sales Engineer from Festo) at the new filling system.
© Festo SE & Co. KG
2024/05/06
|
Globale, Allemagne
A real modular DNA factory
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate ...
Lire le communiqué de presse
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate change, pests and diseases threaten plant breeding. To help develop resistant seeds and make them available to agriculture, plant breeders need vast amounts of DNA. That is precisely why Synchron Lab has developed the "DNA factory", which is automated with handling gantries, electric axes, pneumatic grippers and sensors from Festo.
2023/10/11
|
Belgique, Irlande, Pays-Bas, Grande-Bretagne
New CMMT-ST from Festo offers big savings
Machine builders no longer need to choose between a stepper or servo drive, thanks to the CMMT-ST from Festo. ...
Lire le communiqué de presse
Machine builders no longer need to choose between a stepper or servo drive, thanks to the CMMT-ST from Festo. This new extra low voltage servo drive is capable of open or closed loop positioning, which effectively bridges the gap between stepper and servo drives. This means the user can tailor the CMMT-ST to suit the needs of the application and reap the benefits of both control formats.
CMMT-ST
Stepper or Servo? The new CMMT-ST from Festo gives the best of both worlds
Gearbox SMS image 4
SMS communiceert via IO-Link en is een ‘van de plank’ product
2023/07/20
|
Belgique, Pays-Bas
Druivencontrole versneld door vision, AI en SMS
Karsten Europe verzorgt de distributie van druiven uit Afrika en controleert de kwaliteit van dit kwetsbare ...
Lire le communiqué de presse
Karsten Europe verzorgt de distributie van druiven uit Afrika en controleert de kwaliteit van dit kwetsbare product sinds kort volledig automatisch via een vision/AI-systeem van Gearbox. Naast geavanceerde hard- en software bevindt zich in het hart van deze machine ook de Simplified Motion Series van Festo waarmee producten die niet voldoen aan de ingestelde kwaliteitsstaandaarden beheerst naar een parallelbaan worden geduwd. Gearbox koos bewust voor ...
Gearbox SMS image 3
De tijdspanne tussen beoordeling door de AI en de beslissing goed- of afkeur, slechts 0,3 seconde.