© Festo SE & Co. KG
2025/04/28
|
Irlande, Grande-Bretagne
Optimised stepper motor family from Festo
Innovation in stepper motor technology means the gap between stepper and servo technology is narrowing. In ...
Lire le communiqué de presse
Innovation in stepper motor technology means the gap between stepper and servo technology is narrowing. In applications where the performance of a servo motor is not required because there are no highly dynamic loads or high speed demands, the stepper (with its choice of battery-less encoders and motor brakes) offers closed loop positioning.
© Festo SE & Co. KG
Extra low voltage system 2
Festo’s starter kit contains a CMMT-ST servo drive controller with multi-protocol function, an EMMT-ST stepper motor and matching motor/encoder cables.
© Festo SE & Co. KG
Extra low voltage system 1
Festo’s EMMB-ST and EMMT-ST stepper motor family: in combination with the CMMT-ST servo drive controller, it offers users a coordinated servo system at an attractive price.
© Festo SE & Co. KG
2025/03/20
|
Irlande, Grande-Bretagne
Top tips to improve your next electric drive system’s performance
Electric automation can deliver enhanced efficiency, consistency and precision over traditional pneumatics in ...
Lire le communiqué de presse
Electric automation can deliver enhanced efficiency, consistency and precision over traditional pneumatics in many industrial automation applications. However, simple oversights during design and specification can cause serious problems, turning your electric automation dream into the ‘axis of all evil’, according to industrial automation specialist Festo.
© Festo SE & Co. KG
Top tips to improve electric drive performance image 2
Festo’s electronic sizing tool can help specifiers and machine builders to factor in key application parameters to optimise electric drive component selection.
Top tips to improve electric drive performance image 1
Simple oversights during design and specification of electric drives can cause sub-optimal machine performance and premature failure, says Festo.
2024/03/17
|
Irlande, Grande-Bretagne
New ELGD mechanical axis series from Festo
Machine builders and systems installers are under pressure to deliver high performance automation solutions ...
Lire le communiqué de presse
Machine builders and systems installers are under pressure to deliver high performance automation solutions that are quicker to deploy and offer a low total cost of ownership. Industrial automation specialist Festo has developed its new ELGD mechanical axis series to meet these demands. Specifically designed for tooth belt and ball screw mechanical axes in cartesian handling systems, the ELGD series features a simplified design that delivers ...
ELGD 2
Cartesian and pick and place solutions for small parts handling are one of many applications that will benefit from the new Festo ELGD axis series.
ELGD 1
Festo’s new ELGD mechanical axis series provide excellent rigidity, large feed forces and high precision in any electro-mechanical automation task and are available in standard and wide profiles.