Gearbox SMS image 2
Het controleproces start met punnets met druiven die via een transportband in de machine onder de camera door worden gevoerd.
Gearbox SMS image 1
Druivencontrole versneld door vision, AI en SMS
2023/01/15
|
Irlande, Grande-Bretagne
Festo automation technology aids restoration of Notre-Dame Cathedral
Rapid leaps in innovation characterise the development of additive manufacturing processes. Rotterdam-based ...
Lire le communiqué de presse
Rapid leaps in innovation characterise the development of additive manufacturing processes. Rotterdam-based company Concr3de has been working on a 3D printer for stone for more than five years, developing an inkjet technique to participate in the reconstruction of Notre-Dame Cathedral in Paris. They achieved this aim using automation technology from Festo.
Concr3de 2
The Festo ELGA actuator can have a positive pressure applied internally to prevent the ingress of dust: a critical factor in 3D stone printing.
Concr3de 1
Evert Kranendonk of Concr3de and Jeroen te Brake of Festo with the 3D printed striga for Notre-Dame Cathedral
© Festo SE & Co. KG
2022/11/11
|
Globale
Playing it safe in the assembly of MRI machines
The future belongs to human-robot cooperation. System builder BEC developed such a collaborative solution for ...
Lire le communiqué de presse
The future belongs to human-robot cooperation. System builder BEC developed such a collaborative solution for Siemens Healthineers. It inserts coils weighing several tonnes precisely into the magnets of magnetic resonance imaging (MRI) machines. Electric cylinders from Festo, which ensure the coils are securely gripped, play a crucial role here.  
© Festo SE & Co. KG
BEC – Supports with electric cylinders
Flexible, robust and precise: the supports with electric cylinders from Festo need to be powerful enough to be able to hold the coils weighing up to 1.5 tonnes, but at the same time not so powerful that they damage them.
© Festo SE & Co. KG
BEC – High-tech gripper system
High-tech gripper system on the articulated arm robot. It is vital that the coils do not twist or slip when the gripper picks them up and inserts them into the magnets; the tolerance for inserting the coils into the magnets is no more than 0.5...
© Festo SE & Co. KG
BEC – Insertion of coils into the magnets
Collaborative solution: coils weighing several tonnes are inserted precisely into the magnets of magnetic resonance imaging machines.
© Festo SE & Co. KG
2022/10/19
|
Globale
Festo’s new ELGT cantilever electro-mechanical drive
Industrial automation specialist Festo has introduced a new cantilever electro-mechanical drive that is ...
Lire le communiqué de presse
Industrial automation specialist Festo has introduced a new cantilever electro-mechanical drive that is designed to meet the demanding specifications of modern production facilities. The new ELGT drive combines precision with high load-bearing capacity and rigidity, which makes it ideal for small parts and Lithium-ion battery manufacturing.