© Festo SE & Co. KG
Jürgen Lochner, CSO/CTO chez ILLIG
  "Le développement de solutions d'emballage durables est une priorité pour les experts de notre centre technologique ILLIG", déclare Jürgen Lochner, directeur des ventes / directeur de la technologie chez ILLIG Maschinenbau GmbH & Co. KG.
© Festo SE & Co. KG
Système de manutention de piles ILLIG avec axes Festo EGC-HD
Système de manutention de piles : selon ILLIG, les axes électriques EGC-HD avec guidage pour charges élevées pour des vitesses et une précision élevées ainsi que l'axe cantilever extrêmement rigide ELCC du système d'axes modulaire de Festo...
© ILLIG Maschinenbau GmbH & Co. KG
Système de thermoformage ILLIG RDF 85
  Système avec interface d'outil adaptative et variable : la flexibilité de la nouvelle machine de thermoformage RDF 85 de la ligne de produits RedLine permet d'installer des systèmes d'outils de concurrents sur le marché.
© ILLIG Maschinenbau GmbH & Co. KG
ILLIG thermoformed packaging
One thing ILLIG is particularly proud of is the ILLIG Technology Center: here, the company works with manufacturers of branded goods and packaging from the food and non-food area to test new packaging materials and shapes.
© Festo SE & Co. KG
2022/04/29
|
Globale
On the safe side
With the tubing PUN-H-F and the stainless-steel push-in fitting NPQR, manufacturers of food and packaging ...
Lire le communiqué de presse
With the tubing PUN-H-F and the stainless-steel push-in fitting NPQR, manufacturers of food and packaging machines are on the safe side. This product combination from Festo guarantees compliance with food safety requirements. But Festo has suitable tubing/fitting combinations for other extreme situations too.
© Festo SE & Co. KG
Tubing PUN-H-F with push-in fitting NPQR
On the safe side: The combination of the tubing PUN-H-F and the stainless-steel push-in fitting NPQR from Festo guarantees compliance with food safety requirements for manufacturers of food and packaging machines.
© Festo SE & Co. KG
Tubing PUN-H-F
Tubing PUN-H-F: For highly versatile use in food applications, the “natural” colour variant can also be used in applications with gaseous oxygen.
2021/10/20
|
Irlande, Grande-Bretagne
Grolsch bottling plant upgrade goes with a swing, thanks to Festo automation
New servo technology from Festo is helping Grolsch to put the iconic swing tops on its bottles of lager. The ...
Lire le communiqué de presse
New servo technology from Festo is helping Grolsch to put the iconic swing tops on its bottles of lager. The ‘swing-top transfer unit’ was custom-designed by Festo in conjunction with system integrator MCA Linear Motion Robotics and is installed at the Grolsch Enschede plant in The Netherlands.
© Festo SE & Co. KG
Grolsch pic 2
The Grolsch 'swing-top transfer unit' features the new Festo EMMT servo motor and CPX-E automation system and provides approximately 3,800 bottles per hour with a porcelain cap and rubber ring.