© Festo SE & Co. KG
2023/03/13
|
Globale
How to control precisely very small volumes of liquid
Dispensing, aspirating, pipetting – precision is a must when handling very small volumes of liquid. So ...
Lire le communiqué de presse
Dispensing, aspirating, pipetting – precision is a must when handling very small volumes of liquid. So how do specialists in laboratory automation manage to meet their quality requirements reliably and efficiently, even with high throughputs? How do they achieve reproducible results and avoid contamination? The Life Science webinar from automation specialist Festo provides clear answers to these and many other questions. When? On Wednesday, 16 ...
© Festo SE & Co. KG
Dispense head VTOI for microwell plates
Increases dispensing and aspirating throughput: the precise 8-channel dispense head for microwell plates.
© Festo SE & Co. KG
2021/04/07
|
Globale
Compact, versatile, powerful
Dosing, aspirating or continuous flow – with the media-separated valves VYKA, VYKB and VZDB from Festo ...
Lire le communiqué de presse
Dosing, aspirating or continuous flow – with the media-separated valves VYKA, VYKB and VZDB from Festo all three operating modes are possible. The compact yet powerful valves dose and aspirate even small quantities with a high level of precision. Thanks to their impressive pressure and nominal width specifications, they are also suitable for controlling the flow in a manifold duct plate, for example.
© Festo SE & Co. KG
Solenoid valves VYKA, VYKB and VZDB
Dosing, aspirating or continuous flow – with the media-separated valves VYKA, VYKB and VZDB from Festo all three operating modes are possible.
SupraCube
© Festo SE & Co. KG
SupraCube on a transport system
The SupraCube is a Compact stand-alone levitation module with superconductor technology.
SupraCube
© Festo SE & Co. KG
2021/04/12
|
Globale
SupraCube: Maximum flexibility in automation technology
With the SupraCube, Festo is presenting for the first time a SupraMotion concept in which the superconductor ...
Lire le communiqué de presse
With the SupraCube, Festo is presenting for the first time a SupraMotion concept in which the superconductor unit can be separated from the electrical cooler and can operate autonomously for up to two hours. The compact technology allows contactless movement and handling of objects - ideal for industries with the highest requirements for cleaning and cleanliness, such as laboratory automation, biotechnology or semiconductor production.
French translation unavailable for Festo Introduces a Miniature Valve for In-Vitro Diagnostics, Point-of-Care Devices, and Labs on a Chip .