© Festo SE & Co. KG
2024/02/15
|
Globale
Moving loads at the tip of two fingers
Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in assembly and ...
Lire le communiqué de presse
Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in assembly and logistics to lift and move loads effortlessly, using just two fingers. At the heart of the balancer is the powerful and reliable drive solution YHBP from Festo with automatic weight detection and safety Performance Level d – perfect for the automotive and packaging industries.
© Festo SE & Co. KG
2023/11/14
|
Irlande, Grande-Bretagne
New electric parallel gripper from Festo
Modern manufacturing requires handling solutions capable of managing product diversity, shorter product life ...
Lire le communiqué de presse
Modern manufacturing requires handling solutions capable of managing product diversity, shorter product life cycles and growing levels of product customisation. The HEPP electric gripper from Festo addresses this need for greater flexibility in the gripping of multiple workpieces with adaptable stroke lengths and gripping forces.
© Festo SE & Co. KG
HEPP electric parallell gripper
Compact, simple, precise: the powerful HEPP electric gripper from Festo.
© Festo SE & Co. KG
2023/11/08
|
Globale
Bénéficier de plusieurs fonctionnalités au sein d'un seul et même ...
Ouvrir des récipients d'échantillons et pipeter des échantillons liquides dans le ...
Lire le communiqué de presse
Ouvrir des récipients d'échantillons et pipeter des échantillons liquides dans le même espace de travail ? C’est possible !  Le nouveau portique multi-axes EXCL de Festo équipé d’une petite surface au sol pour les appareils de table et d’une commande de mouvement basée sur PCB permet un réel gain de place au sein d’un laboratoire.
© Festo SE & Co. KG
2024/05/06
|
Globale, Allemagne
A real modular DNA factory
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate ...
Lire le communiqué de presse
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate change, pests and diseases threaten plant breeding. To help develop resistant seeds and make them available to agriculture, plant breeders need vast amounts of DNA. That is precisely why Synchron Lab has developed the "DNA factory", which is automated with handling gantries, electric axes, pneumatic grippers and sensors from Festo.
Gearbox SMS image 4
SMS communiceert via IO-Link en is een ‘van de plank’ product
2023/07/20
|
Belgique, Pays-Bas
Druivencontrole versneld door vision, AI en SMS
Karsten Europe verzorgt de distributie van druiven uit Afrika en controleert de kwaliteit van dit kwetsbare ...
Lire le communiqué de presse
Karsten Europe verzorgt de distributie van druiven uit Afrika en controleert de kwaliteit van dit kwetsbare product sinds kort volledig automatisch via een vision/AI-systeem van Gearbox. Naast geavanceerde hard- en software bevindt zich in het hart van deze machine ook de Simplified Motion Series van Festo waarmee producten die niet voldoen aan de ingestelde kwaliteitsstaandaarden beheerst naar een parallelbaan worden geduwd. Gearbox koos bewust voor ...
Gearbox SMS image 3
De tijdspanne tussen beoordeling door de AI en de beslissing goed- of afkeur, slechts 0,3 seconde.