© Festo SE & Co. KG
Festo Automation Platform (AP)
The Festo Automation Platform (AP) provides the utmost in topology flexibility. All the distributed and decentralized I/O are under a single IP address.
© Festo SE & Co. KG
Festo Motion Control Package (FMCP)
The Festo Motion Control Package (FMCP) control panel arrives wired and ready for installation. This image shows the full edition cabinet that houses up to six drives, the compact panel houses three drives.
© Festo SE & Co. KG
2024/02/15
|
Globale
Moving loads at the tip of two fingers
Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in assembly and ...
Lire le communiqué de presse
Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in assembly and logistics to lift and move loads effortlessly, using just two fingers. At the heart of the balancer is the powerful and reliable drive solution YHBP from Festo with automatic weight detection and safety Performance Level d – perfect for the automotive and packaging industries.
© Festo SE & Co. KG
Jan Seyler
Jan Seyler, Head of Advanced Development Analytics and Control at Festo: "Our many years of experience in the fields of mechanics, logistics and industrial automation, as well as our AI expertise as a team, have enabled us to develop this complete...
© Adolf Würth GmbH & Co. KG
Roland Schneider, Würth
Roland Schneider, Head of the Technical Department at Würth.: "An advantage of the Festo solution is that it requires no teaching or training. Just do it, just get started. It also works with any robot and vision system, making us flexible in our...
© Adolf Würth GmbH & Co. KG
Johannes Scheuermann, Würth
Johannes Scheuermann, Head of Inventory Management at Würth: "We were impressed by the team spirit and the high level of expertise of the developers and researchers at Festo. We are convinced that this project will enable us to significantly...
© Festo SE & Co. KG
2024/04/24
|
Globale
Pneumatics Makes a Technological Leap with Piezo
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new ...
Lire le communiqué de presse
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new perspectives for pneumatics. Thanks to this technology, the pressure control of the compact proportional valve terminal VTEP is extremely sensitive, down to less than 1 mbar. This is perfect for applications such as wafer polishing or patch clamping in life science. In addition, Controlled Pneumatics uses high-precision piezo valves to reduce ...
© Festo SE & Co. KG
VTEP - use in patch clamping
With the VTEP, it is possible to implement applications such as patch clamping human cells using pressure and vacuum.
© Festo SE & Co. KG
VTEP - use in battery production
The VTEP is suitable for the web control of battery foils, for example.