Portugal is the cork world champion: with the largest acreage under cork oaks, the Portuguese are also the largest cork exporters worldwide. Although cork itself is light, it is all the more voluminous if it is packaged inefficiently. In order to save energy and CO₂ emissions during transport, the ESI Group developed a system for packaging corks that requires 30 per cent less packaging volume and does without plastic. On board: automation technology from Festo. Leggi communicato stampa Immagine Festo SE & Co. KG 2022/05/27 | Globale Save 30 per cent volume Portugal is the cork world champion: with the largest acreage under cork oaks, the Portuguese are ... Leggi communicato stampa
Indonesia wants to become one of the ten leading economies by 2030. The way to achieve this is through the digital transformation of the Indonesian industry. Festo is a strong partner in the government programme “Making Indonesia 4.0”. For more than 30 years, the company has had its own local national company and supports the competitiveness of all domestic industries, such as food, automotive, textiles, pharmaceuticals and electronics, with customised automation and qualification solutions. Leggi communicato stampa Immagine Festo SE & Co. KG 2021/04/12 | Global „We make Indonesia 4.0“ Indonesia wants to become one of the ten leading economies by 2030. The way to achieve this is ... Leggi communicato stampa