© Festo SE & Co. KG
SupraCube ready for use
Once cooled and disconnected from the cooler, the SupraCube is ready for use: connected in parallel with other SupraCubes on a transport system or for use in the safety lab next door.
SupraCube
© Festo SE & Co. KG
SupraCube on a transport system
The SupraCube is a Compact stand-alone levitation module with superconductor technology.
© Festo SE & Co. KG
2021/04/12
|
Globale
„We make Indonesia 4.0“
Indonesia wants to become one of the ten leading economies by 2030. The way to achieve this is through the ...
Leggi comunicato stampa
Indonesia wants to become one of the ten leading economies by 2030. The way to achieve this is through the digital transformation of the Indonesian industry. Festo is a strong partner in the government programme “Making Indonesia 4.0”. For more than 30 years, the company has had its own local national company and supports the competitiveness of all domestic industries, such as food, automotive, textiles, pharmaceuticals and electronics, ...
© Festo Didactic
Bionic Swift project-based approach
Project-based approach in class: explore topics such as lightweight construction, energy efficiency and aerodynamics together as a team. 
© Festo Didactic SE
Bionic Swift agile flight behaviour
The ultra-light Bionic Swift shows a particularly agile flight behaviour.
© Festo Didactic SE
Bionic Swift remote radio control
Playful learning: experience the flight characteristics of the Bionic Swift using remote radio control. 
© Festo Didactic SE
Bionic Swift experimental kit
Bionic Swift: The experimental kit that lets you experience bird flight and the world of bionics in a hands-on way. 
SupraCube
© Festo SE & Co. KG
2021/04/12
|
Globale
SupraCube: Maximum flexibility in automation technology
With the SupraCube, Festo is presenting for the first time a SupraMotion concept in which the superconductor ...
Leggi comunicato stampa
With the SupraCube, Festo is presenting for the first time a SupraMotion concept in which the superconductor unit can be separated from the electrical cooler and can operate autonomously for up to two hours. The compact technology allows contactless movement and handling of objects - ideal for industries with the highest requirements for cleaning and cleanliness, such as laboratory automation, biotechnology or semiconductor production.
© Festo SE & Co. KG
Simbolo dell'elettromobilità
Nel 2020, Festo è riuscita ad aumentare le vendite nel segmento "macchine e sistemi per la produzione di batterie" del 40%, e vede grandi opportunità di ulteriore crescita.