© Festo SE & Co. KG
BEC – High-tech gripper system
High-tech gripper system on the articulated arm robot. It is vital that the coils do not twist or slip when the gripper picks them up and inserts them into the magnets; the tolerance for inserting the coils into the magnets is no more than 0.5...
Japanese translation unavailable for Teste dosatrici e portali di movimentazione Festo in uso.
Japanese translation unavailable for Fino a 50 antibiotici contemporaneamente sul banco di prova.
Japanese translation unavailable for Salvare vite con l'antibiotico giusto.
Japanese translation unavailable for Gefit e Festo: partnership per crescere nel segno dell'innovazione tecnologica.
Japanese translation unavailable for MBL Solutions protagonista nella produzione di mascherine chirurgiche e FFP2.
VEMD: proportional control valve pic 2
Extremely high control dynamics: the VEMD proportional flow control valve is ideal for regulating gas flows in ventilation treatment.
VEMD: proportional control valve
The new VEMD proportional flow control valve from Festo offers extremely high control dynamics combined with minimal space and power consumption requirements.  
Agitazione, movimenti improvvisi della bocca: il robot umanoide simula il possibile comportamento dei bambini durante un trattamento dentale.
© tmsuk, Japan
2023/03/13
|
ワールドワイド
No longer afraid of the dentist
No one enjoys going to the dentist; young children even less so. To help future dentists and dental assistants ...
プレスリリースを閲覧する
No one enjoys going to the dentist; young children even less so. To help future dentists and dental assistants deal with children during dental treatments, the Japanese company tmsuk has developed a humanoid robot that realistically simulates the behaviour of young children during these treatments, complete with fidgeting, flinching or closing the mouth. The dummy’s realistic movements are produced using proportional pressure regulators with ...