© Festo SE & Co. KG
VTEP - use in patch clamping
With the VTEP, it is possible to implement applications such as patch clamping human cells using pressure and vacuum.
© Festo SE & Co. KG
SPS 2023
Bringing automation to life at the SPS 2023! Experience the latest highlights of electric automation and be inspired by our resource-efficient approaches!
© Festo SE & Co. KG
2024/05/07
|
ワールドワイド
Many functions safe under the roof of VTUX
Festo is now making it even easier for its users: the functions of the classic valve terminals CPV, MPA-L/S and ...
プレスリリースを閲覧する
Festo is now making it even easier for its users: the functions of the classic valve terminals CPV, MPA-L/S and VTUG are now available under the umbrella of the convertible valve terminal VTUX. In addition, the AP-I and AP-A communication system creates the ideal platform for digitalized production. This brings flexibility and openness - true to the motto "Open Architecture".
© Festo SE & Co. KG
VTUX
VTUX: The new valve terminal combines the advantages of three classic valve terminals (photo: Festo)
© Festo SE & Co. KG
2023/12/05
|
ワールドワイド
Eichenberger convinces compared to products from the Chinese market
Eichenberger successfully held its own against local Chinese manufacturers in the planning of the new Festo ...
プレスリリースを閲覧する
Eichenberger successfully held its own against local Chinese manufacturers in the planning of the new Festo gripper due to outstanding quality (5000% more operational performance in the endurance test), production from a single source, years of expertise and close cooperation throughout the development process from start to finish.   
© Festo SE & Co. KG
Gripper HEPP
Gripper HEPP with spindle from Eichenberger
© Festo SE & Co. KG
2023/11/08
|
ワールドワイド, ドイツ語
A mass flow controller that is silent, fast and cost-effective
 For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow ...
プレスリリースを閲覧する
 For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow controller from Festo delivers maximum control dynamics and costs significantly less than comparable solutions for the control of air, oxygen and inert gases.
© Festo SE & Co. KG
Sensapex - PGVA-2 pressure and vacuum generator from Festo
For Sensapex, an important component for delivering well controlled and reliable application of pressure is the decentralized pressure and vacuum generator PGVA-2 from Festo.
© Festo SE & Co. KG
Festo Experience Center 2
Festo Experience Center bieten die Möglichkeit, innovativen Kundenservice im Kontext der Digitalisierung voranzutreiben.