© Festo SE & Co. KG
2023/07/19
|
アメリカ合衆国
Festo Brings Automated Sample and Liquid Handling Solutions to AACC 2023
Festo features at AACC 2023 Cartesian gantry systems for handling samples and a flexible, high accuracy liquid ...
プレスリリースを閲覧する
Festo features at AACC 2023 Cartesian gantry systems for handling samples and a flexible, high accuracy liquid dispensing system, that enables manufacturers to reduce engineering and procurement overhead while speeding time to market. (Festo AACC [American Association for Clinical Chemistry] Booth #4457, July 23-27, Anaheim Convention Center, Anaheim, Calif.)
© Festo SE & Co. KG
2023/08/04
|
カナダ
Saving lives with low-cost molecular diagnostic tests, with Festo on board
The Fast MDx testing system is not only a game-changer in pathogen detection, it promises to be a life saver. ...
プレスリリースを閲覧する
The Fast MDx testing system is not only a game-changer in pathogen detection, it promises to be a life saver. Available starting in June, Fast MDx is the world’s first fully automated, high-throughput, near-patient molecular diagnostic testing system.  Developed by the London, England-based social enterprise company of the same name with engineering support and automation technology from Festo, this extremely compact, mobile platform cuts ...
© Festo SE & Co. KG
2024/05/06
|
ワールドワイド
Extremely high sample throughput rates
If there’s one thing the corona pandemic has taught us, it is that laboratories place tremendous ...
プレスリリースを閲覧する
If there’s one thing the corona pandemic has taught us, it is that laboratories place tremendous importance on high sample throughput rates. Even with highly qualified laboratory personnel, this demand can no longer be met. There’s no getting round the automation of laboratory processes. That’s why MolGen in the Netherlands developed PurePrep TTR, which can prepare 320 patient samples per hour for molecular downstream processing. And ...
© Festo SE & Co. KG
DHOE pipetting head
An open pipetting system with pipetting head DHOE for simple liquid transport makes it possible to configure the most important pipetting functions based on requirements, and to expand them flexibly – the system is also compatible with the largest...
© Festo SE & Co. KG
MolGen - Pipetting
Extremely small pipetting volumes: the second robot arm with the pipetting head distributes liquids onto a microwell plate.
© Festo SE & Co. KG
MolGen - Opening vial
During the initial work operation, the first robot arm grasps a sample vial by the cap with an electric gripper and brings it into a position at which the cap is removed.
© Festo SE & Co. KG
MolGen - Gripping vial
During the initial work operation, the first robot arm grasps a sample vial by the cap with an electric gripper and brings it into a position at which the cap is removed.
© Festo SE & Co. KG
MolGen - PurePrep TTR
High throughput: the fully automated PurePrep TTR system prepares 320 patient samples per hour for PCR testing. Laboratory-specific automation technology from Festo is included.
Japanese translation unavailable for The New Festo Solution for DeltaV DCS Expands Integration Options and Productivity.