© Festo SE & Co. KG
2023/02/10
|
ワールドワイド
Saving lives worldwide with low-cost molecular diagnostic tests
Fast MDx shows how many pathogens can be detected with unrivalled speed without the need for expensive ...
プレスリリースを閲覧する
Fast MDx shows how many pathogens can be detected with unrivalled speed without the need for expensive biosecure laboratories. This near-patient testing system, developed by London-based company Fast MDx, cuts the typical 24 to 48 hour waiting time to just one to two hours. The new system uses automation technology from Festo.
© Festo SE & Co. KG
Fast MDx - Richard Lewis
Richard Lewis, founder and CEO of Fast MDx.
© Festo SE & Co. KG
Fast MDx - operator
After manual placement, operators can focus on their actual task, namely analysing the results.
© Festo SE & Co. KG
Fast MDx - gripping
Fully automated tests: a separate handling system, based on the EXCM-30 planar surface gantry, uses electric griper EHPS-16 to transport and position the microwell plate between the individual processing steps.
© Festo SE & Co. KG
Fast MDx - pipetting 2
The automated pipetting system, consisting of the pipetting head DHOE from Festo and the disposable syringe ejector DHAO, can accurately dispense volumes in the range of 10 µl.
© Festo SE & Co. KG
Fast MDx - pipetting 1
Space-saving: one gantry each takes care of pipetting and dispensing liquids as well as transporting and positioning the microwell plate.
© Festo SE & Co. KG
Fast MDx - testing system
High throughput: two 3D gantries with pipetting and transport units ensure a fully automated sequence of molecular diagnostic tests.
© Festo SE & Co. KG
2022/11/11
|
ワールドワイド
Playing it safe in the assembly of MRI machines
The future belongs to human-robot cooperation. System builder BEC developed such a collaborative solution for ...
プレスリリースを閲覧する
The future belongs to human-robot cooperation. System builder BEC developed such a collaborative solution for Siemens Healthineers. It inserts coils weighing several tonnes precisely into the magnets of magnetic resonance imaging (MRI) machines. Electric cylinders from Festo, which ensure the coils are securely gripped, play a crucial role here.  
© Festo SE & Co. KG
BEC – Cooperation with Festo
Hans-Günther Nusseck, project manager at BEC (left), and Timo Kloker, sales engineer at Festo, discussing the use of the Festo electric cylinders in the system.
© Festo SE & Co. KG
BEC – Hans-Günther Nusseck
Hans-Günther Nusseck, project manager at BEC