© Festo SE & Co. KG
Cobot E30
Magswitch E-Series intelligent magnetic grippers reduce end-effector size, lower cycle time, ensure safety, and offer new solutions. Shown here is the CoBot SmartMagGrip E30 for collaborative robotic applications.Magswitch E-Series intelligent...
© Festo SE & Co. KG
2021/11/15
|
ワールドワイド
The right handling system in a matter of minutes
With the Handling Guide Online, design engineers can create the right ready-to-install handling system from ...
プレスリリースを閲覧する
With the Handling Guide Online, design engineers can create the right ready-to-install handling system from Festo in record time, whether for a 2D linear and planar surface gantry, a 3D gantry or a new 3D cantilever system. Not only can they now plan extremely compact or extremely dynamic Cartesian robots using the intuitive configuration and ordering software, but they also benefit from the circuit diagram service from Eplan and commissioning files.
© Festo SE & Co. KG
Handling Guide Online
With the Handling Guide Online, machine and system builders are able to reduce their time to market for integrated handling systems by up to 70%.
© Festo SE & Co. KG
2023/05/15
|
ワールドワイド
Reliable degassing in battery cell production
Degassing and sealing are core processes in battery cell production that directly follow the initial contacting ...
プレスリリースを閲覧する
Degassing and sealing are core processes in battery cell production that directly follow the initial contacting of the battery cells with electrical voltage. The battery cells are pierced with lances and the forming gas produced during contacting is extracted. Pneumatic and electric actuators from Festo are used to handle and pierce the battery cells.
© Festo SE & Co. KG
ViscoTec – applying of thermal paste
Maximum dispensing precision with systems from market leader ViscoTec, whether gluing smartphone displays and mini cameras or applying thermal paste.
© Festo SE & Co. KG
SDBT proximity switch
The proximity switch SDBT-MSX with auto teach-in learns the piston end position itself once installed in the approximate position.
© Festo SE & Co. KG
2022/05/23
|
ワールドワイド
Servo-pneumatic welding guns from Festo reduce downtimes by 25 percent
A leading car manufacturer has been relying on the pinpoint accuracy and efficiency of servo-pneumatic welding ...
プレスリリースを閲覧する
A leading car manufacturer has been relying on the pinpoint accuracy and efficiency of servo-pneumatic welding guns from Festo for many years. So much so that they have now installed more than 2,500 welding gun robots with this technology in the premium brand’s body shops. This car manufacturer has now been able to reduce downtimes by 25 percent thanks to a predictive maintenance system from Festo which is ready for artificial intelligence.
© Festo SE & Co. KG
Dashboard Predictive Maintenance
Everything in sight: dashboards for predictive maintenance offer an overview of the machine status.
© Festo SE & Co. KG
Predictive Maintenance for welding guns
Reduce downtimes by 25 percent with servo-pneumatic welding guns from Festo – ready for artificial intelligence.