© Festo SE & Co. KG
VFOE one-way flow control valve
Barely thicker than a tube – the one-way flow control valve VFOE.
© Festo SE & Co. KG
Valves VHEF and VMEF
Manually and mechanically actuated valves VHEF and VMEF from Festo
© Festo SE & Co. KG
2021/05/24
|
ワールドワイド
Precise and robust
The essence of any mechanical switching device is an accurate response. That is exactly why it is designed to ...
プレスリリースを閲覧する
The essence of any mechanical switching device is an accurate response. That is exactly why it is designed to respond with precision. And why it can be installed, without backlash, in just a few steps. The manually and mechanically actuated valves from the VHEF and VMEF series from Festo follow precisely these mechanical principles.
© Festo SE & Co. KG
Valve VHEF
The universal, manual stem actuated valve with pushbutton, switch, hand lever or toggle lever attachment.
Japanese translation unavailable for Festo Introduces a Miniature Valve for In-Vitro Diagnostics, Point-of-Care Devices, and Labs on a Chip .
Japanese translation unavailable for New Festo VMEF/VHEF manual or mechanically actuated valves deliver great precision.
© Festo SE & Co. KG
VAEM valve controller
Small, light, energy efficient, fast, and precise ‒ the VAEM overcomes the challenges found in micro-dispensing liquids.
Agitazione, movimenti improvvisi della bocca: il robot umanoide simula il possibile comportamento dei bambini durante un trattamento dentale.
© tmsuk, Japan
2023/03/13
|
ワールドワイド
No longer afraid of the dentist
No one enjoys going to the dentist; young children even less so. To help future dentists and dental assistants ...
プレスリリースを閲覧する
No one enjoys going to the dentist; young children even less so. To help future dentists and dental assistants deal with children during dental treatments, the Japanese company tmsuk has developed a humanoid robot that realistically simulates the behaviour of young children during these treatments, complete with fidgeting, flinching or closing the mouth. The dummy’s realistic movements are produced using proportional pressure regulators with ...
© Festo SE & Co. KG
VEAA/VEAB proportional pressure regulator
Silent, smooth and fast thanks to piezo technology: the VEAA/VEAB proportional pressure regulator.
Agitazione, movimenti improvvisi della bocca: il robot umanoide simula il possibile comportamento dei bambini durante un trattamento dentale.
© tmsuk, Japan
Pedia Roid Simulation of dental treatment 2
Fidgeting, twitching or sudden closing of the mouth: The humanoid robot for training purposes simulates the possible behaviour of children during a dental treatment.