© tmsuk, Japan
Pedia Roid Simulation of dental treatment 1
The Pedia Roid robot for training dentists and dental assistants: Piezo technology simulates lifelike movements.
Japanese translation unavailable for Festo Introduces a Unique Valve Manifold with Integrated Safety and EtherNet/IP Connectivity .
© Festo SE & Co. KG
IO link pyramid
IO-Link: With controllers, valve terminals, proportional valves and sensors, Festo offers a complete range of IO-Link-capable automation technology.
© Festo SE & Co. KG
2022/09/20
|
ワールドワイド
Nereda® technology for footprint and energy savings
The patented Nereda process from Royal HaskoningDHV offers wastewater treatment plants that take up 75% less ...
プレスリリースを閲覧する
The patented Nereda process from Royal HaskoningDHV offers wastewater treatment plants that take up 75% less space than conventional plants, require just 50% of the energy and are also odour-free, while delivering excellent purification performance. Pneumatic automation technology from Festo ensures reliable and exact process sequences, while experts from Festo provide support with planning the plant.
© Festo SE & Co. KG
Process valve unit
Pre-assembled process valve units ensure that the components match one another properly, make installation easier and give you planning certainty, even in the case of customer-specific solutions.
© Festo SE & Co. KG
Valve terminal CPX-VTSA with bus module
Valve terminal CPX-VTSA with the new bus module CPX-FB44/45: Festo has upgraded its PROFINET bus interfaces for the CPX automation platform.
© Festo SE & Co. KG
VUVG assembly line
Festo’s two-step production concept: In the first step, the Global Production Centers produce the basic product components efficiently and in high quantities. This production step is tailored to worldwide demand and does not tend to be linked to...
© Festo SE & Co. KG
Technology plant Scharnhausen
Festo’s two-step production concept: In the first step, the Global Production Centers produce the basic product components efficiently and in high quantities. This production step is tailored to worldwide demand and does not tend to be linked to...
© Festo SE & Co. KG
Assembly 1
In manufacturing and assembly, employees work according to the Festo Value Production system (FVP). This defines international standards for operating processes within value creation chains and is based on closely involving employees in defining...