2019/02/28
BionicSoftArm
Whether free and flexible movements or defined sequences, the modular pneumatic lightweight robot can be ...
© Festo SE & Co. KG
BionicSoftHand and BionicCobot at a workstation
The BionicSoftHand - mounted on the BionicCobot - can interact safely and directly with humans and support them in assembly tasks, for example.
© Festo SE & Co. KG
BionicSoftHand with dodecahedron
The BionicSoftHand should rotate a 12-sided “cube” (dodecahedron) so that a previously defined side points upwards at the end.  
© Festo SE & Co. KG
2020/03/06
|
ワールドワイド
Pneumatic robotics meets artificial intelligence
Whether its grabbing, holding or turning, touching, typing or pressing – in everyday life, we use our ...
プレスリリースを閲覧する
Whether its grabbing, holding or turning, touching, typing or pressing – in everyday life, we use our hands as a matter of course for the most diverse tasks. In that regard, the human hand, with its unique combination of power, dexterity and fine motor skills, is a true miracle tool of nature. What could be more natural than equipping robots in collaborative workspaces with a gripper that is modelled after this model of nature, that solves ...
© Festo SE & Co. KG
BionicFinWave
The fins of the BionicFinWave are cast out of silicone and do not require struts or support elements.
© Festo SE & Co. KG
BionicFinWave
The underwater robot BionicFinWave manoeuvres itself independently through a pipe system made of acrylic glass.
Supra Drive 2.0
© Festo SE & Co. KG
SupraDrive 2.0
With superconductor technology, objects can be stored and moved without contact – as with the SupraDrive 2.0.
SupraMultitool
© Festo SE & Co. KG
SupraMultitool
At the SupraMultitool exhibit, a handling system positions a workpiece carrier on two different magnets in turn.
BionicWorkplace
© Festo SE & Co. KG
BionicWorkplace_2
Sensors and camera systems register the positions of the operator, components and tools at the BionicWorkplace.
BionicWorkplace
© Festo SE & Co. KG
BionicWorkplace_3 Sprachsteuerung
Humans can intuitively control the BionicCobot in the BionicWorkplace by means of gestures, touch or speech.