BionicWorkplace
© Festo SE & Co. KG
BionicWorkplace_1
BionicWorkplace: A human works together with a bionic robotic arm, along with numerous assistance systems and peripheral devices that are conntected and communicate with each other.
SupraModule
© Festo SE & Co. KG
SupraModule_4
With the SupraModule, different applications can be carried out with the same system in a floating position and controlled wirelessly. Depending on requirements, different systems can be attached to the carrier, for example a compact gripper.
SupraModule
© Festo SE & Co. KG
SupraModule_3
With the SupraModule, different applications can be carried out with the same system in a floating position and controlled wirelessly. Depending on requirements, different systems can be attached to the carrier, for example a compact gripper.
SupraModule
© Festo SE & Co. KG
SupraModule_2
With the SupraModule, different applications can be carried out with the same system in a floating position and controlled wirelessly. Depending on requirements, different systems can be attached to the carrier, for example a compact gripper.
SupraModule
© Festo SE & Co. KG
SupraModule 1
With the SupraModule, different applications can be carried out with the same system in a floating position and controlled wirelessly. Depending on requirements, different systems can be attached to the carrier, for example a compact gripper.
SupraModule
© Festo SE & Co. KG
2023/03/13
|
ワールドワイド
SupraModule: Modulare Lösung für die Laborautomation
In future-oriented fields such as laboratory automation or biotechnology the requirements placed on the ...
プレスリリースを閲覧する
In future-oriented fields such as laboratory automation or biotechnology the requirements placed on the cleaning of production facilities and their purity are very high. With superconductor technology, objects can be moved and handled without contact, which is ideal for such applications. At the Hannover Messe 2020 trade fair, Festo will be presenting the SupraModule concept, which enables wireless control of functions on a magnetic, floating carrier ...
BionicWorkplace
© Festo SE & Co. KG
BionicWorkplace mit Robotino
The constant automatic feed of material in the BionicWorkplace is ensured by a Robotino®, which autonomously travels back and forth between the stations and safely finds its way by means of a laser scanner. It is loaded by a refined version of the...
SupraSensor
© Festo SE & Co. KG
SupraSensor: Messen mit Supraleitung
The concept SupraSensor allows various physical quantities, such as weight, density, viscosity or temperature, to be measured using a force-based measuring system.
SupraSensor
© Festo SE & Co. KG
SupraSensor
SupraSensor: contactless measuring and weighing with superconductor technology.
© Festo SE & Co. KG
BionicSoftArm 2
The BionicSoftArm as a classic SCARA application with a pick-and-place task: it can work in the tightest of spaces around obstacles.