Lange en complexe engineering-, programmeer- en inbedrijfstellingsfasen vertragen veel bedrijven. Met Festo AX Controls presenteert Festo een real-time automatiseringsplatform dat precies dit probleem aanpakt. Het combineert besturing, motion, AI, data-integratie en voorspellend onderhoud in een flexibele, schaalbare oplossing - perfect afgestemd op de eisen van de moderne industrie. Persbericht lezen Afbeelding Festo S.E. & Co. KG 2026/01/28 | Wereldwijd Festo AX Controls geeft automatisering een nieuwe ... Lange en complexe engineering-, programmeer- en inbedrijfstellingsfasen vertragen veel bedrijven ... Persbericht lezen
Digitalisation and artificial intelligence (AI) are megatrends that can also offer great potential for savings in tyre production. Machine learning algorithms can be implemented in a decentralised manner, for example on the edge, i.e. on the actual module to be monitored. An example is Festo AX. This AI software uses these algorithms to detect anomalies on tyre building machines or in curing presses. Persbericht lezen Afbeelding Festo SE & Co. KG 2023/03/17 | Wereldwijd Optimising curing presses with AI Digitalisation and artificial intelligence (AI) are megatrends that can also offer great potential ... Persbericht lezen
With the Handling Guide Online, design engineers can create the right ready-to-install handling system from Festo in record time, whether for a 2D linear and planar surface gantry, a 3D gantry or a new 3D cantilever system. Not only can they now plan extremely compact or extremely dynamic Cartesian robots using the intuitive configuration and ordering software, but they also benefit from the circuit diagram service from Eplan and commissioning files. Persbericht lezen Afbeelding Festo SE & Co. KG 2021/11/15 | Wereldwijd The right handling system in a matter of minutes With the Handling Guide Online, design engineers can create the right ready-to-install handling ... Persbericht lezen
Choosing the right drive technology in automation saves money and, at the same time, also protects the climate. So how do users find the right technology that enables them to reduce carbon dioxide emissions in the long term? The new CO₂ & TCO Guide from Festo supports machine and system manufacturers to make the choice. Persbericht lezen Afbeelding Festo SE & Co. KG 2021/10/07 | Global Selection tool saves money and reduces CO₂ ... Choosing the right drive technology in automation saves money and, at the same time, also protects ... Persbericht lezen
2026/04/24 | Global Interpack 2026 7. tot 13 mei 2026, Messe Düsseldorf Persberichten (7) Afbeeldingen (16) Persmap bekijken Afbeelding Festo SE & Co. KG