© Festo SE & Co. KG
ILLIG stack handling system with Festo axes EGC-HD
Stack handling system: according to ILLIG, the electric axes EGC-HD with heavy-duty guide for high speeds and precision as well as the extremely rigid cantilever axis ELCC from Festo’s modular axis system proved to have the very high precision and...
Frugalpac 3
De unieke lijm- en bevochtingsoplossing helpt Frugalpac om de gewenste cyclustijden van 630 flessen per uur te halen door in batches van acht flessen tegelijk te lijmen.
© Festo SE & Co. KG
Frugalpac 2
De automatiseringscel voor Frugal Bottle werd ontworpen door PCE Automation met behulp van Festo’s Handling Guide Online (HGO) voor snellere ontwerp- en leveringstijden.
Frugalpac 1
Festo automatisering helpt bij vergroten van de productie van Frugal Bottle, de eerste papieren fles voor wijn en sterkedrank ter wereld.
© Festo SE & Co. KG
2021/11/15
|
Wereldwijd
The right handling system in a matter of minutes
With the Handling Guide Online, design engineers can create the right ready-to-install handling system from ...
Persbericht lezen
With the Handling Guide Online, design engineers can create the right ready-to-install handling system from Festo in record time, whether for a 2D linear and planar surface gantry, a 3D gantry or a new 3D cantilever system. Not only can they now plan extremely compact or extremely dynamic Cartesian robots using the intuitive configuration and ordering software, but they also benefit from the circuit diagram service from Eplan and commissioning files.
© Festo SE & Co. KG
Handling Guide Online
With the Handling Guide Online, machine and system builders are able to reduce their time to market for integrated handling systems by up to 70%.
2021/10/20
|
Ierland, Groot-Brittannië
Grolsch bottling plant upgrade goes with a swing, thanks to Festo automation
New servo technology from Festo is helping Grolsch to put the iconic swing tops on its bottles of lager. The ...
Persbericht lezen
New servo technology from Festo is helping Grolsch to put the iconic swing tops on its bottles of lager. The ‘swing-top transfer unit’ was custom-designed by Festo in conjunction with system integrator MCA Linear Motion Robotics and is installed at the Grolsch Enschede plant in The Netherlands.
© Festo SE & Co. KG
Grolsch pic 2
The Grolsch 'swing-top transfer unit' features the new Festo EMMT servo motor and CPX-E automation system and provides approximately 3,800 bottles per hour with a porcelain cap and rubber ring.
Grolsch pic 1
New servo technology from Festo is helping Grolsch to put the iconic swing tops on its bottles of lager.