VEFC
Once a setpoint is set, the Festo VEFC mass flow controller maintains it without hysteresis. The VEFC delivers up to 200 l/min flow and is one of the most compact units on the market.
© Festo SE & Co. KG
2025/01/15
|
Kanada, USA
Festo Introduces the VTUX, the Company’s new Flagship Valve Terminal
Festo introduces its new flagship valve terminal, the VTUX. The VTUX can serve as I/O, remote I/O, and ...
Czytaj informację prasową
Festo introduces its new flagship valve terminal, the VTUX. The VTUX can serve as I/O, remote I/O, and decentralized I/O. These compact and rugged IP65/67-rated terminals can be located anywhere on a machine that boosts operational performance and original equipment manufacturer (OEM) installation productivity. VTUX modularity results in less inventory and lower overhead costs. Slated to replace Festo’s legacy terminals, the VTUX will be the ...
© Festo SE & Co. KG
VTUX
The VTUX valve terminal assembled as remote I/O with the CPX-AP-A communications module, left, I/O, center, and two subbases with a total of eight valve slices, right. Each terminal can have up to 128 valves.
© Festo SE & Co. KG
Individual polishing chambers
The variable contact pressure of the individual polishing chambers is controlled precisely using VTEP. This ensures excellent results, even when polishing wafers.
© Festo SE & Co. KG
Best control for dancer rollers
The VTEP provides the best control for dancer rollers in web tensioning applications.
© Festo SE & Co. KG
Target reached
The “motion complete” function, familiar from electric drive technology, is now also available for pneumatic pressure control as “target reached.”
© Festo SE & Co. KG
VTEP
The world’s first proportional valve terminal, the VTEP, provides closed-loop control of moderate air flow on up to 10 channels. It is ultra compact, measuring less than five inches wide.
vorausrobotik
© Festo SE & Co. KG
2024/11/08
|
Świat
Festo AX Controls automation portfolio in use
Fresh on the market, the Festo AX Controls automation portfolio is showing its open side: voraus robotik, an ...
Czytaj informację prasową
Fresh on the market, the Festo AX Controls automation portfolio is showing its open side: voraus robotik, an innovative software company from Hanover, is integrating its automation software into Festo AX Controls. With the software voraus.core, manufacturers, integrators and end users can easily create and execute solutions for a wide range of applications and optimize and monitor their entire automation.
AX Controls
© Festo SE & Co. KG
2024/11/08
|
Świat
More customer success through seamless data accessibility
Users today face the challenge of having to integrate different topics such as control and motion, AI, data ...
Czytaj informację prasową
Users today face the challenge of having to integrate different topics such as control and motion, AI, data integration and evaluation, predictive maintenance and much more into their applications at the same time, with short development cycles and ever new requirements. Festo AX Controls presents an automation portfolio that takes these requirements into account. The motto "from the workpiece to the cloud" is taken further here, and Festo AX ...