2024/06/27
|
Irlandia, Wielka Brytania
New sensor from Festo
The new SFAM, from industrial automation specialist Festo, is a pressure and flow sensor combined in one ...
Czytaj informację prasową
The new SFAM, from industrial automation specialist Festo, is a pressure and flow sensor combined in one compact unit. Equipped with IO-Link®, the SFAM sensor enables data-driven insights and reduces the number of components required, so system designers and machine builders can save time, space and cost. It also simplifies stocking and provides greater design flexibility.
SFAM sensor
The new SFAM from Festo is a pressure and flow sensor combined in one unit.
© Festo SE & Co. KG
2024/06/24
|
Italië
Cilindro a doppio effetto ADN e ADN-S
Tra le soluzioni Core Product Range Festo troviamo gli attuatori compatti a doppio o semplice effetto della ...
Czytaj informację prasową
Tra le soluzioni Core Product Range Festo troviamo gli attuatori compatti a doppio o semplice effetto della serie ADN e ADN-S. La serie ADN segue la norma ISO 21287 con oltre 350 varianti, ed è disponibile in diverse taglie: dal diametro 12 al 125mm, con corse standard fino a 500mm e differenti tipologie di ammortizzazione. Il profilo è dotato di tre facce con scanalature a T per alloggiare un sensore di finecorsa delle serie SMT-8M-A e ...
© Festo SE & Co. KG
2024/06/06
|
Świat
Festo Expands its Portfolio with Multilayer Manifolds
Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to ...
Czytaj informację prasową
Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to be able to offer manufacturers of medical and laboratory equipment solutions from a single source. To this end, Festo is taking over the production systems and processes for manufacturing these complex plastic manifolds from Carville, a leading company in this field.
© Festo SE & Co. KG
Multilayer Manifold
Multilayer manifolds for manufacturers of medical and laboratory equipment: in future, Festo will offer these in combination with media-separated valves from a single source. 
© Festo SE & Co. KG
Battery Recycling
Recovering valuable lithium, cobalt, manganese and nickel from used batteries and reuse them for the production of new batteries: Automated recycling processes enable these rare minerals to be reused economically and cleanly. Festo has the right...
Polish translation unavailable for Sensore di portata SFAM.