Faster time-to-market, more efficient engineering, more functionality and higher quality – these are the benefits of a digital twin for machine and system builders. Festo is working hard to equip its automation components with a digital twin – a digital representation in the form of administration shells. The company has joined forces with other German automation partners and the Industrial Digital Twin Association because standardisation is what machine and system builders expect. Read press release Image Festo SE & Co. KG 2024/03/08 | Global Digital twins boost machine development Faster time-to-market, more efficient engineering, more functionality and higher quality – these are ... Read press release
Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in assembly and logistics to lift and move loads effortlessly, using just two fingers. At the heart of the balancer is the powerful and reliable drive solution YHBP from Festo with automatic weight detection and safety Performance Level d – perfect for the automotive and packaging industries. Read press release Image Festo SE & Co. KG 2024/02/15 | Global Moving loads at the tip of two fingers Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in ... Read press release
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new perspectives for pneumatics. Thanks to this technology, the pressure control of the compact proportional valve terminal VTEP is extremely sensitive, down to less than 1 mbar. This is perfect for applications such as wafer polishing or patch clamping in life science. In addition, Controlled Pneumatics uses high-precision piezo valves to reduce compressed air consumption by up to 50%. Read press release Image Festo SE & Co. KG 2024/02/05 | Global Pneumatics Makes a Technological Leap with Piezo Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up ... Read press release
"Our aim is to achieve a high level of maturity of CNC machines with our additive manufacturing machines," explains Dr. Vino Suntharakumaran, Managing Director at DMG MORI Additive GmbH. The company is not far off reaching this aim with the LASERTEC 30 DUAL SLM, which increases productivity by 80%. Festo has been brought on board as a development partner. Thanks to its ready-to-install automation solution, the inert gas atmosphere is precisely managed. Read press release Image Festo SE & Co. KG 2024/01/15 | Global 80% more productivity in 3D printing "Our aim is to achieve a high level of maturity of CNC machines with our additive manufacturing ... Read press release
At the award ceremony on 23 November in Düsseldorf, Festo was presented with the German Sustainability Award (DNP) in the hydraulics, pumps and compressors category. The DNP is based on the goals of the German government's Agenda 2030 and thus on key areas of transformation such as climate, biodiversity, resources, supply chain and society. Festo was also recently named a successful practice company in the field of sustainability by RWTH Aachen University and the Complexity Management Academy. Read press release Image Festo SE & Co. KG 2023/11/24 | Global Festo honoured with German Sustainability Award At the award ceremony on 23 November in Düsseldorf, Festo was presented with the German ... Read press release
The industrial, trade and construction sectors have been using the SCHUKO plug, invented by ABL in 1925, for almost 100 years. The company can now produce more than 100 versions of SCHUKO plugs and couplings quickly and flexibly on a new assembly system supplied by special machine builder AS Automation. This is also made possible by the highly flexible Multi-Carrier-System MCS® as well as numerous other electric and pneumatic automation products from Festo. Read press release Image Festo SE & Co. KG 2023/11/11 | Global More than 100 versions on one system The industrial, trade and construction sectors have been using the SCHUKO plug, invented by ABL in ... Read press release
Festo is now making it even easier for its users: the functions of the classic valve terminals CPV, MPA-L/S and VTUG are now available under the umbrella of the convertible valve terminal VTUX. In addition, the AP-I and AP-A communication system creates the ideal platform for digitalized production. This brings flexibility and openness - true to the motto "Open Architecture". Read press release Image Festo SE & Co. KG 2023/11/11 | Global Italy Many functions safe under the roof of VTUX Festo is now making it even easier for its users: the functions of the classic valve terminals CPV ... Read press release
Eichenberger successfully held its own against local Chinese manufacturers in the planning of the new Festo gripper due to outstanding quality (5000% more operational performance in the endurance test), production from a single source, years of expertise and close cooperation throughout the development process from start to finish. Read press release Image Festo SE & Co. KG 2023/11/10 | Global Eichenberger convinces compared to products from ... Eichenberger successfully held its own against local Chinese manufacturers in the planning of the ... Read press release
For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow controller from Festo delivers maximum control dynamics and costs significantly less than comparable solutions for the control of air, oxygen and inert gases. Read press release Image Festo SE & Co. KG 2023/11/09 | Global Germany A mass flow controller that is silent, fast and ... For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass ... Read press release
The extremely compact rotary gripper module EHMD is the ideal choice in many life science applications where small objects need to be gripped and turned in confined spaces. For example, it can be used in laboratory automation to open a variety of sample vials with ease. The Z module automatically adjusts to the thread pitches of the caps, eliminating changeover times. Read press release Image Festo SE & Co. KG 2023/11/08 | Global Reliably gripping and turning small parts The extremely compact rotary gripper module EHMD is the ideal choice in many life science ... Read press release
Opening sample vessels and pipetting liquid samples in the same workspace saves space in laboratories. This can now be achieved with the three-dimensional gantry EXCL from Festo, which has a small footprint for table-top devices and PCB-based motion control. Read press release Image Festo SE & Co. KG 2023/11/08 | Global Multiple functions in a small workspace Opening sample vessels and pipetting liquid samples in the same workspace saves space in ... Read press release
Dosing, aspirating and controlling extremely small quantities of aggressive liquids and gases is not a problem with the media-separated solenoid valve VYKA from Festo. This compact powerhouse has a width of only 7 mm and can dose and aspirate the extremely small amounts of liquid very precisely. It also meets the strict requirements for leak-tightness for gas applications. Read press release Image Festo SE & Co. KG 2023/11/08 | Global Compact and leak-tight powerhouse Dosing, aspirating and controlling extremely small quantities of aggressive liquids and gases is not ... Read press release
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate change, pests and diseases threaten plant breeding. To help develop resistant seeds and make them available to agriculture, plant breeders need vast amounts of DNA. That is precisely why Synchron Lab has developed the "DNA factory", which is automated with handling gantries, electric axes, pneumatic grippers and sensors from Festo. Read press release Image Festo SE & Co. KG 2023/11/08 | Global Germany A real modular DNA factory Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population ... Read press release
Higher demands on throughput and precision – this is only possible with more automation in laboratory technology. Sensapex already equips more than 800 customers worldwide with high-precision micromanipulators, microscopes, and pressure controllers – from neuroscience research to in vitro fertilization (IVF) – to name only a few application examples. To work successfully the pressure controllers from Sensapex rely on the decentralized pressure and vacuum generator PGVA from Festo. Read press release Image Sens 2023/11/08 | Global Germany Ensuring the right pressure Higher demands on throughput and precision – this is only possible with more automation in ... Read press release
In Europe, Germany's mechatronics experts are simply top: at the European Skills Championship EuroSkills Gdańsk 2023 in Poland last September, Daniel Schmid and Timo Oßwald, both apprentices at Festo, won the gold medal in the skill mechatronics. They thus completed the extremely successful record of the German national team, which came second behind Switzerland in the 'Best of Nations' ranking in 42 trades. Read press release Image WorldSkills Germany 10/20/2023 | Global Simply top in Europe In Europe, Germany's mechatronics experts are simply top: at the European Skills Championship ... Read press release
Siemens Xcelerator, the open digital business platform, creates an open ecosystem for collaboration between customers, Siemens, and certified partners, from large technology companies to independent software developers. Festo and Siemens announced their latest partnership at this year’s Hannover Messe trade fair. Festo has joined the Industrial Edge Ecosystem. To kick this off, Festo is offering the Festo AX Data access app, effective immediately, on the Siemens Industrial Edge Marketplace, where industrial customers can purchase numerous apps... Read press release Image Festo SE & Co. KG 09/21/2023 | Global Festo joins the Siemens Industrial Edge ecosystem Siemens Xcelerator, the open digital business platform, creates an open ecosystem for collaboration ... Read press release