If there’s one thing the corona pandemic has taught us, it is that laboratories place tremendous importance on high sample throughput rates. Even with highly qualified laboratory personnel, this demand can no longer be met. There’s no getting round the automation of laboratory processes. That’s why MolGen in the Netherlands developed PurePrep TTR, which can prepare 320 patient samples per hour for molecular downstream processing. And the Dutch company uses laboratory-specific automation technology from Festo. Read press release Image Festo SE & Co. KG 2023/04/24 | Global Extremely high sample throughput rates If there’s one thing the corona pandemic has taught us, it is that laboratories place tremendous ... Read press release
The Festo Group achieved double-digit growth for another year in a row. Sales rose by 13.4% to €3.81 billion in 2022 (previous year €3.36 billion). Festo intends to continue growing in 2023. Innovative automation is the enabler for the industrial transformation towards renewable energies, sustainable production, hydrogen and circular economy. Read press release Image Festo SE & Co. KG 2023/04/17 | Global Festo continues on course for growth and ... The Festo Group achieved double-digit growth for another year in a row. Sales rose by 13.4% to €3.81 ... Read press release
The production of tyres and the production of wafers seem to have absolutely nothing to do with each other. In terms of automation technology, however, they use the same technology: Controlled Pneumatics. That is why Festo has further developed compressed air technology to make pneumatics sustainable, resource-saving and energy-efficient. Read press release Image Festo SE & Co. KG 2023/04/17 | Global Moving into the future with Controlled Pneumatics The production of tyres and the production of wafers seem to have absolutely nothing to do with each ... Read press release
On site and hands-on: At the Hannover Messe, visitors on the Festo booth can use all their senses experience comprehensive learning environments. Highlights of the product portfolio in the field of education and training will be on display – from the digital learning portal Festo LX and virtual reality learning to product innovations in the field of learning systems with cobots, AI and the digital twin. Read press release Image Festo Didactic SE 04/11/2023 | Global Ireland United Kingdom Lifelong learning as a driver of innovation On site and hands-on: At the Hannover Messe, visitors on the Festo booth can use all their senses ... Read press release
At the Hannover Messe 2023, Festo is presenting the next step on the road to the industrialisation of biological transformation: BionicCellFactory. With automation technology from Festo, biomass can be cultivated on a large scale in a highly efficient, resource-conserving way. Everything that we currently produce from crude oil creating immense CO2 emissions can also be obtained sustainably from algae. With the BionicCellFactory, Festo is demonstrating a holistic bioprocess – from the optimised cultivation of the algae with continuous... Read press release Image Festo SE & Co. KG 2023/03/22 | Global Cultivation of biomass on an industrial scale At the Hannover Messe 2023, Festo is presenting the next step on the road to the industrialisation ... Read press release
Digitalisation and artificial intelligence (AI) are megatrends that can also offer great potential for savings in tyre production. Machine learning algorithms can be implemented in a decentralised manner, for example on the edge, i.e. on the actual module to be monitored. An example is Festo AX. This AI software uses these algorithms to detect anomalies on tyre building machines or in curing presses. Read press release Image Festo SE & Co. KG 2023/03/17 | Global Optimising curing presses with AI Digitalisation and artificial intelligence (AI) are megatrends that can also offer great potential ... Read press release
Flexible, robust and offering high performance – the angle seat valve VZXA from Festo controls media flows quickly and reliably up to 230 °C. Its carefully thought-out product design and patented interface enable valve bodies and actuators to be freely combined, with a hot-swap function for quickly exchanging actuator or other spare parts. Read press release Image Festo SE & Co. KG 2023/03/17 | Global Flexible interfaces in plant engineering Flexible, robust and offering high performance – the angle seat valve VZXA from Festo controls media ... Read press release
The twin cylinder DGTZ from Festo is short, flat and extremely versatile. The versatility is ensured by the mounting options on four sides of this rigid and thus non-rotating twin cylinder that is also maintenance-free. Read press release Image Festo SE & Co. KG 2023/03/13 | Global Ideal for tight spaces The twin cylinder DGTZ from Festo is short, flat and extremely versatile. The versatility is ensured ... Read press release
The configurators for process valve and quarter turn actuator units from Festo make it easier for system planners to find the optimal solution. Simply select a few parameters and the configurators will suggest appropriate combinations, making engineering in the process industry fast, reliable and easy with coordinated and ready-to-install solutions. Read press release Image Festo SE & Co. KG 2023/03/13 | Global The quicker way to get process valve and quarter ... The configurators for process valve and quarter turn actuator units from Festo make it easier for ... Read press release
Festo has upgraded its PROFINET bus interfaces for the CPX automation platform. The new generation has four new key features based on the new PROFINET controllers and software, with the “S2 system redundancy” being the most important one. Read press release Image Festo SE & Co. KG 2023/03/13 | Global New PROFINET bus interfaces from Festo Festo has upgraded its PROFINET bus interfaces for the CPX automation platform. The new generation ... Read press release
No one enjoys going to the dentist; young children even less so. To help future dentists and dental assistants deal with children during dental treatments, the Japanese company tmsuk has developed a humanoid robot that realistically simulates the behaviour of young children during these treatments, complete with fidgeting, flinching or closing the mouth. The dummy’s realistic movements are produced using proportional pressure regulators with piezo technology from Festo. Read press release Image tmsuk, Japan 2023/03/13 | Global No longer afraid of the dentist No one enjoys going to the dentist; young children even less so. To help future dentists and dental ... Read press release
BZEE and Festo Didactic renew their longstanding collaboration to offer guidance and learning resources to support training providers in the tuition of skilled wind turbine technicians in order to accelerate the transition to renewable energy. Read press release Image Festo Didactic SE 02/28/2023 | Global Solutions that boost the employability of future ... BZEE and Festo Didactic renew their longstanding collaboration to offer guidance and learning ... Read press release
Read press release Image Festo SE & Co. KG 02/27/2023 | Global Festo Breaks Price/Performance Barriers with New ... Read press release
The term "sustainability" all too often turns into mere lip service. Not so at Wellspect. This world leader in manufacturing solutions for medical continence care has made sustainability an integral part of its corporate strategy and is committed to putting it into practice. No wonder the company’s plant in Mölndal near Gothenburg, Sweden, relies on Festo Energy Saving Services which save Wellspect €37,000 a year in energy costs. Read press release Image Wellspect 2023/02/13 | Global €37,000 less energy costs in medical technology The term "sustainability" all too often turns into mere lip service. Not so at Wellspect. This world ... Read press release
Fast MDx shows how many pathogens can be detected with unrivalled speed without the need for expensive biosecure laboratories. This near-patient testing system, developed by London-based company Fast MDx, cuts the typical 24 to 48 hour waiting time to just one to two hours. The new system uses automation technology from Festo. Read press release Image Festo SE & Co. KG 2023/02/10 | Global Saving lives worldwide with low-cost molecular ... Fast MDx shows how many pathogens can be detected with unrivalled speed without the need for ... Read press release
The sustainability of cardboard packaging is leading to its increasing use instead of plastic packaging. A key step in the manufacture of folding boxes is the highly precise gluing of the box blanks. The company Baumer hhs is a specialist and global market leader for applications of this type with its dual-piston pump DPP – supported by the proportional valve VPPM from Festo. Read press release Image Festo SE & Co. KG 01/25/2023 | Global Ireland United Kingdom Proportional valve technology makes it possible The sustainability of cardboard packaging is leading to its increasing use instead of plastic ... Read press release