© Festo SE & Co. KG
EHMD in laboratory automation
The compact rotary gripper module EHMD from Festo can handle virtually any gripping task in laboratory automation, no matter how small.  
© Festo SE & Co. KG
2024/05/02
|
Global
Reliably gripping and turning small parts
The extremely compact rotary gripper module EHMD is the ideal choice in many life science applications where ...
Ler comunicados de imprensa
The extremely compact rotary gripper module EHMD is the ideal choice in many life science applications where small objects need to be gripped and turned in confined spaces. For example, it can be used in laboratory automation to open a variety of sample vials with ease. The Z module automatically adjusts to the thread pitches of the caps, eliminating changeover times.
© Festo SE & Co. KG
Rotary gripper module EHMD
The compact rotary gripper module EHMD comes in a fully electric version or with a pneumatic gripper.
© Festo SE & Co. KG
2024/05/06
|
Global
Compact and leak-tight powerhouse
Dosing, aspirating and controlling extremely small quantities of aggressive liquids and gases is not a problem ...
Ler comunicados de imprensa
Dosing, aspirating and controlling extremely small quantities of aggressive liquids and gases is not a problem with the media-separated solenoid valve VYKA from Festo. This compact powerhouse has a width of only 7 mm and can dose and aspirate the extremely small amounts of liquid very precisely. It also meets the strict requirements for leak-tightness for gas applications.
© Festo SE & Co. KG
VYKA media-separated solenoid valve
The media-separated solenoid valve VYKA allows the precise dispensing of fluids and the control of liquid flows in manifold duct plates as well as gas flows.
© Festo SE & Co. KG
2024/05/06
|
Global, Alemanha
A real modular DNA factory
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate ...
Ler comunicados de imprensa
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate change, pests and diseases threaten plant breeding. To help develop resistant seeds and make them available to agriculture, plant breeders need vast amounts of DNA. That is precisely why Synchron Lab has developed the "DNA factory", which is automated with handling gantries, electric axes, pneumatic grippers and sensors from Festo.
© Festo SE & Co. KG
Bert Baas, Festo
Bert Baas, Vertriebsingenieur bei Festo
© Festo SE & Co. KG
Synchron - Glenn Dukel
Glenn Dukel, Project and Business Development Manager at Synchron Lab
© Festo SE & Co. KG
Synchron - intensive washing process
Intensive washing process: in this station, dispense head VTOI dispenses a buffer solution several times to remove salts and ethanol from the DNA.